Question
STM32 Discovery+OV2640 image too dark
Posted on October 28, 2013 at 04:14
Hi everybody,
I'm working with OV2640 and i've problem with brightness. I use TFT LCD to display, use config from STM32F4xx_DSP_StdPeriph_Lib ( dcmi_ov2640.c). DMA and DCMI working fine but the image i receive too dark. So, i use :void OV2640_BrightnessConfig(uint8_t Brightness){ OV2640_WriteReg(0xff, 0x00); OV2640_WriteReg(0x7c, 0x00); OV2640_WriteReg(0x7d, 0x04); OV2640_WriteReg(0x7c, 0x09); OV2640_WriteReg(0x7d, Brightness); OV2640_WriteReg(0x7d, 0x00);}to increase brightness but the image still dark. I check datasheet of ov2640 for 0x7c and 0x7d reg but i can't find it. I think the config for this ov2640 is wrong, i want to correct it but they config a lot of regs that doesn't describe in the datasheet. I'm going to contact ovt for these reg setting, hope they answer...