Skip to main content
PPopo.1
Senior
May 16, 2024
Solved

stm32 CAN interrupt not triggering

Hello,

I have waisted 2 days already on trying to figure out why interrupt is not being triggered when using CAN RX.

I started new fresh project just to test the CAN and debug it so there is not much initialized here.

So sending data via CAN works for me but when I want to receive it the interrupt never triggers. I have tried with filter and also without ! (didnt know if that maybe has something to do with it) I also have ground connected to my CAN PEAK so that shouldn't be an issue also. I think I initialized all interrupts correctly. I should also add that I created everything with cube IDE .ioc. Any ideas or help will be appriciated. Here are my files: 

 

my main.c

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "can.h"
#include "gpio.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
CAN_TxHeaderTypeDef TxHeader;
CAN_RxHeaderTypeDef RxHeader;


uint8_t TxData[8];
uint8_t RxData[8];
uint32_t TxMailbox;
int datacheck = 0;




void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
	HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData);
	if (RxHeader.DLC == 2 ){
		datacheck = 1;
	}
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */


 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_CAN1_Init();
 /* USER CODE BEGIN 2 */
HAL_CAN_Start(&hcan1);

//activate the notification
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);



TxHeader.DLC = 2;
TxHeader.IDE = CAN_ID_STD;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.StdId = 0x446;

TxData[0] = 100;
	TxData[1]=10;
	HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox);
	 if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
	 {
		 Error_Handler();
	 }

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 if (datacheck == 1){
		 while(1){
int test = 1;
test++;
		 }
	 }
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 5;
 RCC_OscInitStruct.PLL.PLLN = 32;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/* USER CODE BEGIN 4 */
CAN_RxHeaderTypeDef RxHeader;

uint8_t RxData[8];


/* USER CODE END 4 */

/**
 * @brief Period elapsed callback in non blocking mode
 * @note This function is called when TIM6 interrupt took place, inside
 * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
 * a global variable "uwTick" used as application time base.
 * @PAram htim : TIM handle
 * @retval None
 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* USER CODE BEGIN Callback 0 */

 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM6) {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */

 /* USER CODE END Callback 1 */
}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */


CAN.C

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file can.c
 * @brief This file provides code for the configuration
 * of the CAN instances.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "can.h"

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

CAN_HandleTypeDef hcan1;

/* CAN1 init function */
void MX_CAN1_Init(void)
{

 /* USER CODE BEGIN CAN1_Init 0 */

 /* USER CODE END CAN1_Init 0 */

 /* USER CODE BEGIN CAN1_Init 1 */

 /* USER CODE END CAN1_Init 1 */
 hcan1.Instance = CAN1;
 hcan1.Init.Prescaler = 10;
 hcan1.Init.Mode = CAN_MODE_NORMAL;
 hcan1.Init.SyncJumpWidth = CAN_SJW_2TQ;
 hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
 hcan1.Init.TimeTriggeredMode = DISABLE;
 hcan1.Init.AutoBusOff = DISABLE;
 hcan1.Init.AutoWakeUp = DISABLE;
 hcan1.Init.AutoRetransmission = DISABLE;
 hcan1.Init.ReceiveFifoLocked = DISABLE;
 hcan1.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CAN1_Init 2 */



 CAN_FilterTypeDef canFilterConfig;
 canFilterConfig.FilterActivation = CAN_FILTER_ENABLE; // Enable the filter
 canFilterConfig.FilterBank = 0; // Filter bank number
 canFilterConfig.FilterFIFOAssignment = CAN_FILTER_FIFO0; // FIFO 0
 canFilterConfig.FilterIdHigh = 0x0000; // Accept all IDs
 canFilterConfig.FilterIdLow = 0x0000; // Accept all IDs
 canFilterConfig.FilterMaskIdHigh = 0x0000; // Mask to accept all IDs
 canFilterConfig.FilterMaskIdLow = 0x0000; // Mask to accept all IDs
 canFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; // Mask mode
 canFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; // 32-bit scale
 canFilterConfig.SlaveStartFilterBank = 14; // Start filter bank
 HAL_CAN_ConfigFilter(&hcan1, &canFilterConfig); // Configure the filter








 /* USER CODE END CAN1_Init 2 */

}

void HAL_CAN_MspInit(CAN_HandleTypeDef* canHandle)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(canHandle->Instance==CAN1)
 {
 /* USER CODE BEGIN CAN1_MspInit 0 */

 /* USER CODE END CAN1_MspInit 0 */
 /* CAN1 clock enable */
 __HAL_RCC_CAN1_CLK_ENABLE();

 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**CAN1 GPIO Configuration
 PA11 ------> CAN1_RX
 PA12 ------> CAN1_TX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF9_CAN1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* CAN1 interrupt Init */
 HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
 /* USER CODE BEGIN CAN1_MspInit 1 */

 /* USER CODE END CAN1_MspInit 1 */
 }
}

void HAL_CAN_MspDeInit(CAN_HandleTypeDef* canHandle)
{

 if(canHandle->Instance==CAN1)
 {
 /* USER CODE BEGIN CAN1_MspDeInit 0 */

 /* USER CODE END CAN1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_CAN1_CLK_DISABLE();

 /**CAN1 GPIO Configuration
 PA11 ------> CAN1_RX
 PA12 ------> CAN1_TX
 */
 HAL_GPIO_DeInit(GPIOA, GPIO_PIN_11|GPIO_PIN_12);

 /* CAN1 interrupt Deinit */
 HAL_NVIC_DisableIRQ(CAN1_RX0_IRQn);
 /* USER CODE BEGIN CAN1_MspDeInit 1 */

 /* USER CODE END CAN1_MspDeInit 1 */
 }
}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

interrupt.c 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file stm32l4xx_it.c
 * @brief Interrupt Service Routines.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32l4xx_it.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN TD */

/* USER CODE END TD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/* External variables --------------------------------------------------------*/
extern CAN_HandleTypeDef hcan1;
extern TIM_HandleTypeDef htim6;

/* USER CODE BEGIN EV */

/* USER CODE END EV */

/******************************************************************************/
/* Cortex-M4 Processor Interruption and Exception Handlers */
/******************************************************************************/
/**
 * @brief This function handles Non maskable interrupt.
 */
void NMI_Handler(void)
{
 /* USER CODE BEGIN NonMaskableInt_IRQn 0 */

 /* USER CODE END NonMaskableInt_IRQn 0 */
 /* USER CODE BEGIN NonMaskableInt_IRQn 1 */
 while (1)
 {
 }
 /* USER CODE END NonMaskableInt_IRQn 1 */
}

/**
 * @brief This function handles Hard fault interrupt.
 */
void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */

 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}

/**
 * @brief This function handles Memory management fault.
 */
void MemManage_Handler(void)
{
 /* USER CODE BEGIN MemoryManagement_IRQn 0 */

 /* USER CODE END MemoryManagement_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_MemoryManagement_IRQn 0 */
 /* USER CODE END W1_MemoryManagement_IRQn 0 */
 }
}

/**
 * @brief This function handles Prefetch fault, memory access fault.
 */
void BusFault_Handler(void)
{
 /* USER CODE BEGIN BusFault_IRQn 0 */

 /* USER CODE END BusFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_BusFault_IRQn 0 */
 /* USER CODE END W1_BusFault_IRQn 0 */
 }
}

/**
 * @brief This function handles Undefined instruction or illegal state.
 */
void UsageFault_Handler(void)
{
 /* USER CODE BEGIN UsageFault_IRQn 0 */

 /* USER CODE END UsageFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_UsageFault_IRQn 0 */
 /* USER CODE END W1_UsageFault_IRQn 0 */
 }
}

/**
 * @brief This function handles System service call via SWI instruction.
 */
void SVC_Handler(void)
{
 /* USER CODE BEGIN SVCall_IRQn 0 */

 /* USER CODE END SVCall_IRQn 0 */
 /* USER CODE BEGIN SVCall_IRQn 1 */

 /* USER CODE END SVCall_IRQn 1 */
}

/**
 * @brief This function handles Debug monitor.
 */
void DebugMon_Handler(void)
{
 /* USER CODE BEGIN DebugMonitor_IRQn 0 */

 /* USER CODE END DebugMonitor_IRQn 0 */
 /* USER CODE BEGIN DebugMonitor_IRQn 1 */

 /* USER CODE END DebugMonitor_IRQn 1 */
}

/**
 * @brief This function handles Pendable request for system service.
 */
void PendSV_Handler(void)
{
 /* USER CODE BEGIN PendSV_IRQn 0 */

 /* USER CODE END PendSV_IRQn 0 */
 /* USER CODE BEGIN PendSV_IRQn 1 */

 /* USER CODE END PendSV_IRQn 1 */
}

/**
 * @brief This function handles System tick timer.
 */
void SysTick_Handler(void)
{
 /* USER CODE BEGIN SysTick_IRQn 0 */

 /* USER CODE END SysTick_IRQn 0 */

 /* USER CODE BEGIN SysTick_IRQn 1 */

 /* USER CODE END SysTick_IRQn 1 */
}

/******************************************************************************/
/* STM32L4xx Peripheral Interrupt Handlers */
/* Add here the Interrupt Handlers for the used peripherals. */
/* For the available peripheral interrupt handler names, */
/* please refer to the startup file (startup_stm32l4xx.s). */
/******************************************************************************/

/**
 * @brief This function handles CAN1 RX0 interrupt.
 */
void CAN1_RX0_IRQHandler(void)
{
 /* USER CODE BEGIN CAN1_RX0_IRQn 0 */

 /* USER CODE END CAN1_RX0_IRQn 0 */
 HAL_CAN_IRQHandler(&hcan1);
 /* USER CODE BEGIN CAN1_RX0_IRQn 1 */

 /* USER CODE END CAN1_RX0_IRQn 1 */
}

/**
 * @brief This function handles TIM6 global interrupt, DAC channel1 and channel2 underrun error interrupts.
 */
void TIM6_DAC_IRQHandler(void)
{
 /* USER CODE BEGIN TIM6_DAC_IRQn 0 */

 /* USER CODE END TIM6_DAC_IRQn 0 */
 HAL_TIM_IRQHandler(&htim6);
 /* USER CODE BEGIN TIM6_DAC_IRQn 1 */

 /* USER CODE END TIM6_DAC_IRQn 1 */
}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */



This topic has been closed for replies.
PPopo.1
PPopo.1Best answer
Senior
May 17, 2024

Ok so it works now. I have been trying with the filter only in the CUBE IDE where It doesn't work or at least it doesn't stop at the IRQ request. I pasted filter into VS code into my project and it works fine. Not quite sure what's different bit the IRQ just isn't triggering in CUBE

 

10 replies

mƎALLEm
ST Technical Moderator
May 16, 2024

Hello,

Need to attach your project includig your ioc file.

Also please provide what tranceiver part number you're using? what board are you using: ST or custom board?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
PPopo.1
PPopo.1Author
Senior
May 16, 2024

sorry bout that , I am using STM32L431CBT6 on a custom board. As far as transciever part number goes I dont really know what you mean by that. For CAN sending and reading I am using PEAK system and PEAK VIEW

mƎALLEm
ST Technical Moderator
May 16, 2024

As far as transciever part number goes I dont really know what you mean by that.

This is an important part of the the HW part of the CAN.

Do you have schematics of that custom board?

Also better to attach your project (a very simple project that includes the CAN communication and nothing else).

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
PPopo.1
PPopo.1AuthorBest answer
Senior
May 17, 2024

Ok so it works now. I have been trying with the filter only in the CUBE IDE where It doesn't work or at least it doesn't stop at the IRQ request. I pasted filter into VS code into my project and it works fine. Not quite sure what's different bit the IRQ just isn't triggering in CUBE

 

mƎALLEm
ST Technical Moderator
May 17, 2024

It could be something related to the project config like optimization ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.