Skip to main content
rs11
Associate III
February 23, 2009
Question

STM32 - Burst read external NOR flash

  • February 23, 2009
  • 1 reply
  • 619 views
Posted on February 23, 2009 at 12:13

STM32 - Burst read external NOR flash

    This topic has been closed for replies.

    1 reply

    rs11
    rs11Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:04

    STM32 (Access line, 512KB internal Flash, 48K Internal RAM)

    My system's external flash memory reads have a timing constraint, and hence would like to use burst reads from a synchronous flash. Are there any app note or example source code of the processor configuration for burst reading an external flash in synchronous mode? How to set the number of half-words for the burst read. Thanks for any information.