Skip to main content
NAbun.1
Associate II
March 13, 2024
Solved

STM32 Bootloader Pin Availability

Hello,

I am reading AN2606 and I am wondering if I am interpreting the document correctly. Is table 113 suggesting that the FDCAN bootloader is only available on pins PH13 & PH14 in the STM32H75 series? Since these pins do not exist on the 100 pin packages of the part, is it not possible to use the FDCAN bootloader on 100 pin packages?

Thanks.

This topic has been closed for replies.
TDK
TDKBest answer
March 13, 2024

Correct and correct.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
March 13, 2024

Correct and correct.

"If you feel a post has answered your question, please click ""Accept as Solution""."
STTwo-32
ST Technical Moderator
March 13, 2024

Hello @NAbun.1 

As said @TDK , Booth LQFP100 and LQFP144 does not support the FDCAN bootloader.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.