Skip to main content
16-32micros
Associate III
July 3, 2008
Question

STM32 Bootloader & PC GUI Flash demonstrator

  • July 3, 2008
  • 14 replies
  • 2055 views
Posted on July 03, 2008 at 20:40

STM32 Bootloader & PC GUI Flash demonstrator

    This topic has been closed for replies.

    14 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear all,

    A new PC (Flash Loader) GUI demonstrator for the STM32 bootloader is available on this link :

    http://www.st.com/stonline/products/support/micro/files/um0462.zip

    ;) Enjoy it !

    Regards,

    STOne-32

    sjo
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Had little success on rev A silicon - is it known to work?

    Tried both IAR and Keil boards - currently have no rev B to try.

    Cheers

    sjo

    nicolasfillon9
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Hi,

    I tried it on a B revision of chip on a Keil board and it works fine.

    For those who have a Keil board you can use the attached .hex file.

    BR,

    Nicolas. :D

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear all,

    I confirm that The flow control (RTS & CTS ) is not required. For revA and answering 'sjo' question we have some earlier versions of bootloader

    (1.x) but now the stable version is ''2.0'' and this is available on all revB & Z devices. To version number is available by ''Get Version'' command and is shown in the Flash Loader demonstrator once the connection is done,

    when you would like to select the target.

    Regards, STOne-32

    ivan239955_stm1_st
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Can somebody confirm that hardware flow control (RTS/CTS) is not required?

    I tried to communicate with Flash loader demonstrator (v1.0) from serial port terminal (pretending to be STM32) and it seems to be happy just with 3 wires( Rx,Tx,GND).

    However, when I replied to Get Command (as described AN2606, page 9/33) demonstrator reported error: ''cannot Get BL available commands''

    Ivan

    wuguobing
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    It doesn't work! The chip version is Rev B, Cable doesn't support hardware flow control. (The UART1 works fine.)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear Oliver,

    I recommand you to request your free STM32 new samples using the Free samples from our web site and to move to RevB/Z :D and then Reworking it on you board (very easy if you have a good rework station). Regards,

    STOne32 :o

    sjo
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Would it be possible to obtain a copy for revA silicon?

    spencer_dot_oliver_at_anglia_dot_com

    Regards

    sjo

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear all,

    I confirm that The flow control (RTS & CTS ) is not required. For revA and answering 'sjo' question we have some earlier versions of bootloader

    (1.x) but now the stable version is ''2.0'' and this is available on all revB & Z devices. To version number is available by ''Get Version'' command and is shown in the Flash Loader demonstrator once the connection is done,

    when you would like to select the target.

    Regards, STOne-32

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear Kuni,

    Could you please check if you are not using a wrong target name. In fact, the displayed target name in the 3rd window is the product family name To select your target combobox and choice the used STM32 Package Flash (32, 64 or 128K of flash) reference between the available ones :STM32F10xx6xx ,STM32F10xx8xx, or STM32F10xxBxx

    the default one is the Biggest Package which is ''B'' = 128K . Thank you.

    Here attached a screenshot :o

    STOne-32.

    [ This message was edited by: STOne-32 on 30-11-2007 12:51 ]