STM32 Bootloader firmware write over uart
Hi everybody,
I'm working on a project where I have a pi cm4 connected to a STM32 (during testing we're using a STM32G07 dev board, but production will be using an STM32G03 chip). I've been asked to write a program to allow the cm4 to update the firmware via the uart. I've managed to get the program to reliably access the bootloader and run get, getv, getid, and readmem (for the flash memory). However when I try to run the write memory command it appears to run successfully, but when I read the memory address I just wrote to it returns the original value. I'm fairly certain that the write protection has already been disabled (checked using STM32CubeProgrammer), but I decided to try and run the write unprotect command just encase, but the chip seem to just hang after running the command.
I'm a recent graduate, and this is my first job, so I'm fairly uncertain as to what I'm doing, so it's very possible I'm missing something important. Thanks for any assistance and patients.