Skip to main content
jaroslaw23
Associate II
March 8, 2011
Question

STM32 @ 16Mhz TXCO

  • March 8, 2011
  • 2 replies
  • 653 views
Posted on March 08, 2011 at 21:38

STM32 @ 16Mhz TXCO

    This topic has been closed for replies.

    2 replies

    jaroslaw23
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:27

    Thanks Clive,

    I will write some more when I lunch the Project.

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:27

    Yes this will work, you need to review the clock trees in the reference manual.

    The USBCLK = PLLCLK/1 or PLLCLK/1.5, permitting a 48 MHz or 72 MHz SYSCLK for USB operation. You could also technically run the CPU at 8 or 16 MHz, and have the PLL just run the USB. The AHB, APBx can be a fraction of the SYSCLK.

    The PLL can be driven by HSI/2, HSE, or HSE/2

    An 6 or 12 MHz TCXO would also work.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..