Skip to main content
KayalaSandeep
Associate
September 4, 2024
Question

STM32 as slave in MODBUS showing the busy and error code 06 How to fixit?

As I am working on the stm32G474VETx with LQFP100 packing. For master and slave, I am using same type of board. I am implementing the MODBUS communication using the fiber optic cable but every time I am getting the error code 06 showing that the salve is busy. I am requesting the everyone what is the possible reasons getting the slave in busy state. And mention the how to fix them. I need to operate this in at least in the 1 Mbps to 2. I implementing the MODBUS using the UART Communication. Mention some of the example code implementing MODBUS in stm32 using the polling method, interrupt method and DMA method.

This topic has been closed for replies.