Skip to main content
vaibhavsharma63
Associate II
Jun 8, 2013 10:15 AM UTC
Question

stm32 adc multi channel

Posted on June 08, 2013 at 12:15

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    22 replies

    frankmeyer9
    Associate III
    Jun 13, 2013 11:40 AM UTC
    Posted on June 13, 2013 at 13:40

    Just add some code to initialise  the UART and associated pins, and the send functionality.

    You will find plenty of examples around in the web, google is your friend (well, except if you insist on privacy ...).

    Coocox should maintain a collection of examples, and the StdPeripheralLibrary, as part of the F4 discovery firmware, is available from the ST website. The latter contains examples for all peripherals, including UART:

    vaibhavsharma63
    Associate II
    Jun 13, 2013 12:14 PM UTC
    Posted on June 13, 2013 at 14:14

    this is my code for usart .and i am  facing again one error which i found last time ..please suggest me how to remove it .....code is here

    #include <stm32f4xx_usart.h>

    #include ''stm32f4xx_adc.h''

    #include ''stm32f4xx_gpio.h''

    #include ''stm32f4xx_rcc.h''

    #include ''stm32f4xx.h''

    void init_usart(void){

     GPIO_InitTypeDef GPIO_InitStructure;

     USART_InitTypeDef USART_InitStructure;

     /* enable peripheral clock for USART2 */

     RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

     /* GPIOA clock enable */

     RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

     /* GPIOA Configuration:  USART2 TX on PA2 */

     GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;

     GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

     GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

     GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

     GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;

     GPIO_Init(GPIOA, &GPIO_InitStructure);

     /* Connect USART2 pins to AF2 */

     // TX = PA2

     GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);

     USART_InitStructure.USART_BaudRate = 9600;

     USART_InitStructure.USART_WordLength = USART_WordLength_8b;

     USART_InitStructure.USART_StopBits = USART_StopBits_1;

     USART_InitStructure.USART_Parity = USART_Parity_No;

     USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

     USART_InitStructure.USART_Mode = USART_Mode_Tx;

     USART_Init(USART2, &USART_InitStructure);

     USART_Cmd(USART2, ENABLE); // enable USART2

    }

    void Delay(__IO uint32_t nCount)

    {

      while(nCount--)

      {

      }

    }

    int main(void){

     init_usart();

     uart_puts(''Init complete!'');

     while(1){

      USART_SendData(USART2, 'v'); // defined in stm32f4xx_usart.h

      Delay(0x3FFFFF);

     }

    }

    .ERROR IS HERE

    GCC HOME: C:\Program Files (x86)\GNU Tools ARM Embedded\4.7 2013q1\bin

    compile:

        [mkdir] Created dir: C:\CooCox\CoIDE\workspace\usart\usart\Debug\bin

        [mkdir] Created dir: C:\CooCox\CoIDE\workspace\usart\usart\Debug\obj

           [cc] 18 total files to be compiled.

           [cc] arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -Wall -ffunction-sections -g -O0 -flto -fno-builtin -c -DSTM32F407VG -DSTM32F4XX -DUSE_STDPERIPH_DRIVER -D__ASSEMBLY__ -IC:\CooCox\CoIDE\workspace\usart\cmsis_lib -IC:\CooCox\CoIDE\workspace\usart\cmsis_boot -IC:\CooCox\CoIDE\workspace -IC:\CooCox\CoIDE\workspace\usart\cmsis_lib\include -IC:\CooCox\CoIDE\workspace\usart -IC:\CooCox\CoIDE\workspace\usart\cmsis -IC:\CooCox\CoIDE\workspace\usart\STM32F4-Discovery C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_syscfg.c C:\CooCox\CoIDE\workspace\usart\STM32F4-Discovery\stm32f4_discovery_audio_codec.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_usart.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_dac.c C:\CooCox\CoIDE\workspace\usart\cmsis_boot\startup\startup_stm32f4xx.c C:\CooCox\CoIDE\workspace\usart\STM32F4-Discovery\stm32f4_discovery.c C:\CooCox\CoIDE\workspace\usart\main.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_rcc.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_adc.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_gpio.c C:\CooCox\CoIDE\workspace\usart\cmsis_boot\system_stm32f4xx.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_dma.c C:\CooCox\CoIDE\workspace\usart\stm32f4_discovery_callbacks.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_spi.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_i2c.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\stm32f4xx_exti.c C:\CooCox\CoIDE\workspace\usart\cmsis_lib\source\misc.c C:\CooCox\CoIDE\workspace\usart\STM32F4-Discovery\stm32f4_discovery_lis302dl.c

           [cc] C:\CooCox\CoIDE\workspace\usart\main.c: In function 'main':

           [cc] C:\CooCox\CoIDE\workspace\usart\main.c:59:2: warning: implicit declaration of function 'uart_puts' [-Wimplicit-function-declaration]

           [cc] Starting link

           [cc] arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -g -nostartfiles -flto -Wl,-Map=usart.map -O0 -Wl,--gc-sections -Wl,--entry=main -LC:\CooCox\CoIDE\configuration\ProgramData\usart -Wl,-TC:\CooCox\CoIDE\configuration\ProgramData\usart/arm-gcc-link.ld -g -o usart.elf ..\obj\stm32f4xx_syscfg.o ..\obj\stm32f4_discovery_audio_codec.o ..\obj\stm32f4xx_usart.o ..\obj\stm32f4xx_dac.o ..\obj\startup_stm32f4xx.o ..\obj\stm32f4_discovery.o ..\obj\main.o ..\obj\stm32f4xx_rcc.o ..\obj\stm32f4xx_adc.o ..\obj\stm32f4xx_gpio.o ..\obj\system_stm32f4xx.o ..\obj\stm32f4xx_dma.o ..\obj\stm32f4_discovery_callbacks.o ..\obj\stm32f4xx_spi.o ..\obj\stm32f4xx_i2c.o ..\obj\stm32f4xx_exti.o ..\obj\misc.o ..\obj\stm32f4_discovery_lis302dl.o -L..\..\..\STM32F4-Discovery -lpdmfilter_gcc

           [cc] C:\Users\AKG\AppData\Local\Temp\ccT4as9i.ltrans0.ltrans.o: In function `main':

           [cc] C:\CooCox\CoIDE\workspace\usart/main.c:59: undefined reference to `uart_puts'

           [cc] collect2.exe: error: ld returned 1 exit status

    vaibhavsharma63
    Associate II
    Jun 13, 2013 12:23 PM UTC
    Posted on June 13, 2013 at 14:23

    vaibhavsharma63
    Associate II
    Jun 13, 2013 12:25 PM UTC
    Posted on June 13, 2013 at 14:25

    vaibhavsharma63
    Associate II
    Jun 13, 2013 12:30 PM UTC
    Posted on June 13, 2013 at 14:30

    hello .now i am interfacing pressure sensor (mpx415a) on stm32 discovery board .do u have any sample code in which we can see pressure sensor's data ,

    frankmeyer9
    Associate III
    Jun 13, 2013 12:52 PM UTC
    Posted on June 13, 2013 at 14:52

      [cc] C:\CooCox\CoIDE\workspace\usart/main.c:59: undefined reference to `uart_puts'

     

    You call a function that nowhere exists in the project space.

    Either your toolchain/library supports routing printf()-like functions to UART, or you write it yourself. This forum contains several threads on how to do this with Keil. Not sure what your (undisclosed / gcc-based) toolchain provides.

    Writing it yourself can offer significant code space savings.

    frankmeyer9
    Associate III
    Jun 13, 2013 1:03 PM UTC
    Posted on June 13, 2013 at 15:03

    If you mean a MPX4105A/4115A, this devices have an analog output, and require a +5V supply.

    You will need a buffer amplifier to interface the sensor output with the ADC, to reduce the impedance and to convert the 0..5V sensor output span to 0..3.3V of the ADC.

    Tesla DeLorean
    Guru
    Jun 13, 2013 1:19 PM UTC
    Posted on June 13, 2013 at 15:19

    void uart_puts(char *s)
    {
    while(*s)
    {
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
    USART_SendData(USART2, *s++);
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    raptorhal2
    Lead
    Jun 13, 2013 1:20 PM UTC
    Posted on June 13, 2013 at 15:20

    Minor correction - the F4 Discovery ADC range is 0 to 3V.

    This is a simple exercize for the student.

    Cheers, Hal

    vaibhavsharma63
    Associate II
    Jun 14, 2013 8:42 AM UTC
    Posted on June 14, 2013 at 10:42

    hello .do u have sample code in which pressure sensor working with stm32f4discovery