Skip to main content
Associate III
Jul 31, 2024 8:39 AM UTC
Question

STM Virtual Com port win11 driver needed

hello, where can i download win11 STM virtual com port?  i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din see

STM Virtual Com port at device manager! only STM STLink visual com port appear ... 

12 replies

StanJermAuthor
Associate III
Jul 31, 2024 8:56 AM UTC

i m implementing my own USB VCP on a USB port (STM32 USB Virtual COM Port (VCP) )

https://medium.com/@pasindusandima/stm32-usb-virtual-com-port-vcp-bc7cb1bd5f5

StanJermAuthor
Associate III
Jul 31, 2024 9:03 AM UTC

i m using H734 Nucleo...

AScha.3
Super User
Jul 31, 2024 9:23 AM UTC

Hi,

the VCP driver :

https://www.st.com/en/development-tools/stsw-stm32102.html

should not be needed, as win10 + 11  have driver in system included - so maybe your enumeration going wrong...

or try thr driver - if you want.

 

If you feel a post has answered your question, please click on " Best Answer ".
StanJermAuthor
Associate III
Jul 31, 2024 2:51 PM UTC

hello... anyone can help ???

 

Pavel A.
Jul 31, 2024 4:14 PM UTC

Look for CDC device example in the Cube example projects for STM32H7, adapt it for your board.

 

Andrei Chichak
Lead
Jul 31, 2024 9:42 PM UTC

You don't need a VCP driver for late windows 8 forward. It just shows up as a COM port.

If your device isn't showing up, I'd suggest that there is something incorrect with your program running on the H7. You do have a program running on the H7, don't you? You have to provide a program that implements the device side of the VCP, it's not built into the H7.

StanJermAuthor
Associate III
Aug 1, 2024 3:05 AM UTC

yes.. i hav a program but seems its not working,,,

Visitor II
Mar 27, 2025 10:56 AM UTC

 I am facing similar issue , STM Virtual Com port not appearing at device manager when I  plug usb cable . Were you able to resolve this?

Visitor II
Mar 18, 2026 11:23 AM UTC

Having similar issues with the EVL6482H-Discovery board, latest firmware flashed shows up as a HID compliant barcode reader under windows 11.

HID\VID_0483&PID_7004&REV_0110
HID\VID_0483&PID_7004
HID\VID_0483&UP:008C_U:0001
HID_DEVICE_UP:008C_U:0001

It identifies as a HID compliant device with 2 endpoints