STM USART bootloader issue with STM32F446
I've been using bootloader over USART3 PB10/PB11 at an STM32F446ZET6 for long time and it works reliably at least at 115200kbit.
This year we assembled several new PCB's without HW change and the bootloader stopped working. When programming the STM32 via SWD interface everything seems to work normally - also USART3 communication works fine.
ONLY the bootloader does not answer on char 0x7F
Description: I'm trying to enter the bootloader by hand
- BOOT0pin=high,
- toggle reset of the STM32
- send 0x7F using Hterm terminal in hex mode
Expected result is char 0x79 (or any error byte). But I get no any byte on the fresh controllers. Same test works well on the controllers from last years.
Additional information:
- both, new and old controller initialize USB as DFU interface (so they are not empty, some bootcode must be running)
- old controller bootloader version read out: 3.1
For me it looks like the STM factory boot code has changed since last year. Can you confirm this?
Regards Marten