Skip to main content
werbung
Associate II
Jan 15, 2014 9:55 PM UTC
Question

STM Studio Variables missing

Posted on January 15, 2014 at 22:55

Im using STM Studio 3.3.

When I import my .elf files from Keil or Coocox most of the variables (even direct variables) are missing.

When I analyze the .elf file with nm or eu-nm all the variables are available on fix RAM-adresses and I can manually add these adresses to the read or write list.

What is wrong with importing the .elf files in STM Studio ?

#stm-studio
    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    Jan 24, 2014 10:51 AM UTC
    Posted on January 24, 2014 at 11:51

    Hi Henry,

    Would it be possible to attach your .elf file for check? What are types of missing variables?

    -Mayla-
    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.