Skip to main content
MDeva.1
Associate III
July 23, 2022
Question

STLINK_V3 SET how to use for Custome board?

  • July 23, 2022
  • 1 reply
  • 589 views

Hello,

I am working on STM32H7 . I have custome board , I have to use the STLINK_V3 SET, which things that I need to consider for the programming through STLINK. How much vtg I have to set 3V/5V , In stm32Cube ide which setting I have to make. Can u please help me

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 23, 2022

    The H7 is running at 3V or 3.3V​

    SWD connection, you want SWDIO, SWCLK, NRST and GND.

    Should be able to check connectivity using STM32 Cube Programmer. ​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..