Skip to main content
Jeremy Wong
Associate
January 21, 2018
Question

STEVAL-STLKT01V1 Sensor Tile connect to I2C device

  • January 21, 2018
  • 2 replies
  • 672 views
Posted on January 21, 2018 at 21:54

I have a 

STEVAL-STLKT01V1 Sensor Tile. I want to add additional sensing capabilities and was wondering how to add a peripheral that communicates over I2C? Are there any firmware examples of how to do this?

#stm32l4-hal-i2c
This topic has been closed for replies.

2 replies

Andrew Neil
Super User
January 22, 2018
Posted on January 22, 2018 at 11:40

From UM2101, ''Getting started with the STEVAL-STLKT01V1 SensorTile integrated development platform'':

0690X00000609RuQAI.png

http://www.st.com/resource/en/user_manual/dm00320099.pdf

  

See: 

http://www.st.com/en/evaluation-tools/steval-stlkt01v1.html

 

Just looks to be a standard I2C connection - so any of the STM32 I2C examples should do?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Jeremy Wong
Associate
January 22, 2018
Posted on January 22, 2018 at 16:47

Thanks Andrew for your reply. I was looking at the basic I2C_TwoBoards_ComPolling example from STM32CubeL4 firmware examples but couldn't get it to work. Can you confirm some of the steps?

I2C_ADDRESS - From what I was reading, this should be bit shifted to the left to go from a 7-bit address to 8-bit left justified address? (e.g. I want slave with address 0x04, I would set this as 0x08?)

I2C_TIMING - Not sure how this is calculated so I've been going with the default of 0x00D00E28 from the example. I want the standard 100kbits/s clock rate.

I kept the I2C configurations from the example the same except changed it to 7-bit addressing mode

I2cHandle.Instance = I2Cx;

I2cHandle.Init.Timing = I2C_TIMING;

I2cHandle.Init.OwnAddress1 = I2C_ADDRESS;

I2cHandle.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

I2cHandle.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

I2cHandle.Init.OwnAddress2 = 0xFF;

I2cHandle.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

I2cHandle.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

After that, defining my transmit and receive buffers, I call

HAL_I2C_Master_Transmit(&I2cHandle, (uint16_t)I2C_ADDRESS, (uint8_t*)aTxBuffer, 3, 10000);

HAL_I2C_Master_Receive(&I2cHandle, (uint16_t)I2C_ADDRESS, (uint8_t *)aRxBuffer, 6, 10000);

However, HAL_I2C_Master_Transmit returns HAL_ERROR. I've added 10k resistors to the SDA and SCL lines to pull it up to 5V.

Any ideas what could be going wrong? Thanks.