Skip to main content
Ravide
Visitor II
March 29, 2023
Question

STEVAL PROTEUS-1 - Modal analysis using impact hammer

  • March 29, 2023
  • 0 replies
  • 504 views

Dear all, I'm trying to evaluate the IIS3DWB sensor using the STEVAL PROTEUS-1. Would it be possible to use the sensor to capture transient vibration e.g. Modal test using an impact hammer?

Is there an example script for STEVAL PROTEUS-1, to capture the data and save it to an SD card? The trigger signal will be manually activated prior to the impact and the data will be captured for 60 - 90 seconds. The sampling rate will be a min. of 20kHz as the highest frequency of interest is approx. 7kHz. Any advice would be much appreciated.

Thanks in advance,

best regards,

Ravi

    This topic has been closed for replies.