Skip to main content
Darski.Piotr
Associate II
November 28, 2016
Question

STemWin - WM_SetCreateFlags(WM_CF_MEMDEV) caused problem

  • November 28, 2016
  • 2 replies
  • 923 views
Posted on November 28, 2016 at 14:29

Hello,

I have a problem with my application based on STemWin lib 5.32. Without  WM_SetCreateFlags(WM_CF_MEMDEV) works very fine but there is some flikering. After activation of use memory device 1-2 minuts program is halted. 

How to avoid it? 

regards,

PD
    This topic has been closed for replies.

    2 replies

    slimen
    Visitor II
    November 28, 2016
    Posted on November 28, 2016 at 14:56

    Hello,

    Are you following the

    https://www.segger.com/downloads/emwin/UM03001_emWin5.pdf

    user manual about WM_SetCreateFlags (WM_CF_MEMDEV)

    ''The flag WM_CF_MEMDEV is frequently used to enable Memory Devices on all windows.Setting create flags is permitted before GUI_Init() is called. This causes the backgroundwindow to be also affected by the create flags.

    ''

    Regards

    Darski.Piotr
    Associate II
    November 28, 2016
    Posted on November 28, 2016 at 15:18

    Hi,

    yes I read this issue. Please see my ''main'':int main(void)

    {  

      /* STM32F4xx HAL library initialization:

           - Configure the Flash prefetch, instruction and Data caches

           - Configure the Systick to generate an interrupt each 1 msec

           - Set NVIC Group Priority to 4

           - Global MSP (MCU Support Package) initialization

         */

      HAL_Init();  

      

      /* Configure the system clock to 180 Mhz */

      SystemClock_Config();

      MX_GPIO_Init();

      MX_DMA_Init();                 // !!! by PD

      MX_I2C3_Init();                // !!! by PD   

      MX_I2C1_Init();                // !!! by PD   

      MX_TIM1_Init();                // !!! by PD

      MX_TIM3_Init();                // !!! by PD

      MX_TIM4_Init();                // !!! by PD

      MX_TIM8_Init();                // !!! by PD

      MX_USART1_Init();              // !!! by PD

      MX_FMC_Init();                 // !!! by PD

      FT5206_CTP_BSP_PB_Init();      // !!! by PD  

      MX_RTC_Init();                 // !!! by PD  

      /***********************************************************/

      HAL_TIM_Base_Start_IT(&htim1);

      HAL_TIM_Base_Start_IT(&htim3);

      HAL_TIM_Base_Start_IT(&htim4);  

      HAL_TIM_Base_Start_IT(&htim8);  

      /***********************************************************/

      VARIABLE_INIT();

      

      

      

      /* Init the STemWin GUI Library */

      BSP_SDRAM_Init(); /* Initializes the SDRAM device */

      __CRC_CLK_ENABLE(); /* Enable the CRC Module */

      GUI_Init();

      BSP_Config();

      

      GUI_Initialized = 1;  

      /* Activate the use of memory device feature */

      //WM_SetCreateFlags(WM_CF_MEMDEV);      //here is commented

      MainTask();

        

      while (1)

      {

      }

    }

    WM_SetCreateFlags(WM_CF_MEMDEV) is after GUI_INIT.

    I have STM32F429BIT6 and 4 windows , rest (8) are created and deteted when aplication needs.  

    regards,

    PD