Question
STemWin and external RAM
Posted on April 02, 2015 at 14:37
I have linked STemWin library. My project uses external RAM.
When I display some progressbar using internal RAM, value of progress is displayed correctlly (ex. 50%). When I am switching buffer ''aMemory'' to extrernal RAM (static U32 aMemory[GUI_NUMBYTES / 4] __attribute__ ((section(''.extram''))) the value of progress is displayed strange, ex. 00 instead off 50%, 33 instead of 13%, each times the second digit is shown twice, first digit and ''%'' char aren't displayed. Where is the problem ?