Skip to main content
lanchon
Associate III
Apr 4, 2009 3:08 PM UTC
Question

stdio via USB virtual COM port

Posted on April 04, 2009 at 17:08

stdio via USB virtual COM port

    This topic has been closed for replies.

    48 replies

    anderson
    Visitor II
    Nov 2, 2012 11:57 AM UTC
    Posted on November 02, 2012 at 12:57

    I can't find the attached code. can you provide it?

    anderson
    Visitor II
    Nov 2, 2012 11:59 AM UTC
    Posted on November 02, 2012 at 12:59

    I couldn't find the attached code. could you provided it?

    Tesla DeLorean
    Guru
    Nov 2, 2012 12:09 PM UTC
    Posted on November 02, 2012 at 13:09

    This is a 3 year old thread, before the forum last fatally crashed, the original posters are unlikely to respond.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    viktor
    Visitor II
    Jan 24, 2013 4:49 PM UTC
    Posted on January 24, 2013 at 17:49

    It also seems to be the only example of an USB virtual serial port for STM32 devices that I could find after extensive googling. It would be nice to get hold of it. Alternately I'd appreciate if someone could point me to a complete USB serial port example I can get to work on the F3 or F4 discovery with minimal effort (I know, I should learn the USB spec but you've got to start somewhere).

    asinicki
    Visitor II
    Jan 25, 2013 7:03 PM UTC
    Posted on January 25, 2013 at 20:03

    There is a link on this forum to a COIDE project that uses the VCP.  It is not perfect but it works and is a good place to start.  I had it working with the STM3241G_Eval board in short order.

    http://www.coocox.org/forum/topic.php?id=1757&page=2

    esg
    Associate
    Feb 5, 2013 7:52 AM UTC
    Posted on February 05, 2013 at 08:52

    Hello,

    i am newbe to STM32.and i am using STM32F103C8T6.i have added the USB Lybrary to my code and it was compilled successfully by the gcc compiler(arm-none-eabi).here when i connected my board to PC with USB i am getting ''Unrecognised device''.is there any thing i need to add code after the ''pProperty->Init();'' function call in the USB_Init() function.I also connected a 1.5K pull up at D+ of USB.please help me out someone.

    void USB_Init(void)

    {

      pInformation = &Device_Info;

      pInformation->ControlState = 2;

      pProperty = &Device_Property;

      pUser_Standard_Requests = &User_Standard_Requests;

      /* Initialize devices one by one */

      pProperty->Init();

    ?????????stuck here to add code

    }

    gguerrero9
    Visitor II
    Mar 21, 2013 1:26 PM UTC
    Posted on March 21, 2013 at 14:26

    Hi there,

     I am not able to find attached code :-(, would you please post it again?

    thanks in advance

    Gabriel

    Tesla DeLorean
    Guru
    Mar 21, 2013 1:37 PM UTC
    Posted on March 21, 2013 at 14:37

    I am not able to find attached code :-(, would you please post it again?

     

    No kidding?! This thread is pushing 4 years old before the forum last fatally crashed, the original posters are unlikely to respond. I wish we could lock threads to stop getting questions like this.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..