Skip to main content
o239955_stm1
Associate
December 8, 2017
Question

Start DFU bootloader.

  • December 8, 2017
  • 0 replies
  • 513 views
Posted on December 08, 2017 at 08:32

Hello,

I'm trying to start the DFU bootloader of an STM32F4 Controller.

I have my own bootloader implementation and I try to jump to the DFU bootloader from my bootloader.

My Problem is:

My Firmware is connected to CAN2 of the Controller and there are other modules connected to the CAN-Bus.

I can start the DFU bootloader from my Firmware by Setting a MagicValue in the RAM and perform a Softwarereset.

This starts my own bootloader which reads the MagicValue from the RAM and then starts the DFU bootloader.

It seems that when there is CAN traffic while I want to start the DFU bootlaoder, the DFU bootloader does not start correctly.

Is it possible to tell the DFU bootloader to skip CAN and directly connect to USB-Device?

Additional question:

When starting the DFU bootloader with Keil, what would be the better approach? Starting directly from assembler code or from the main function?

Does anyone know what the __main function does?
    This topic has been closed for replies.