Skip to main content
Associate II
June 26, 2024
Question

STANDBY and SLEEP Modes using RTC

Hello,
I am trying to use the SLEEP and STANDBY modes with the RTC. I want the device to go to sleep/standby mode for 10 seconds and wake up after the 10 seconds are done. I have tried it with an interrupt using UART and Button and both the modes are working fine.But with RTC I am facing an issue.
Can anyone pls help with this query of mine?

Thanking you.

This topic has been closed for replies.

6 replies

ST Employee
June 26, 2024
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
June 27, 2024

Its working for STANDBY Mode.But for SLEEP Mode I am unable to get the core to wake up pls.

HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
	 HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
	 sprintf(date, "Date: %02d.%02d.%02d\t", sDate.Date, sDate.Month, sDate.Year);
	 sprintf(time, "Time: %02d:%02d:%02d\r\n", sTime.Hours, sTime.Minutes, sTime.Seconds);
	 HAL_UART_Transmit(&huart2, (uint8_t *)date, strlen(date), HAL_MAX_DELAY);
	 HAL_UART_Transmit(&huart2, (uint8_t *)time, strlen(time), HAL_MAX_DELAY);

	 // Configure RTC alarm to trigger after 10 seconds
	 RTC_AlarmTypeDef sAlarm;
	 sAlarm.AlarmTime.Hours = 0;
	 sAlarm.AlarmTime.Minutes = 0;
	 sAlarm.AlarmTime.Seconds = 10;
	 sAlarm.Alarm = RTC_ALARM_A;
	 if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BIN) != HAL_OK)
	 {
	 Error_Handler();
	 }

	 // Enter Sleep mode
	 HAL_UART_Transmit(&huart2, (uint8_t *)"MCU is going to sleep...\r\n", strlen("MCU is going to sleep...\r\n"), HAL_MAX_DELAY);
	 HAL_SuspendTick(); // Suspend HAL tick
	 HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFE);

	 // MCU wakes up here

	 // Resume operations after wake-up
	 //SystemClock_Config(); // Restore system clock settings
	 HAL_ResumeTick(); // Resume HAL tick

	 HAL_UART_Transmit(&huart2, (uint8_t *)"MCU woke up from sleep mode\r\n", strlen("MCU woke up from sleep mode\r\n"), HAL_MAX_DELAY);

	 // Delay to avoid immediate sleep cycle
	 HAL_Delay(1000);

...

void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc) {
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);

	 // Print current time and date after wake-up
	 HAL_RTC_GetTime(hrtc, &sTime, RTC_FORMAT_BIN);
	 HAL_RTC_GetDate(hrtc, &sDate, RTC_FORMAT_BIN);
	 sprintf(date, "Date: %02d.%02d.%02d\t", sDate.Date, sDate.Month, sDate.Year);
	 sprintf(time, "Time: %02d:%02d:%02d\r\n", sTime.Hours, sTime.Minutes, sTime.Seconds);
	 HAL_UART_Transmit(&huart2, (uint8_t *)date, strlen(date), HAL_MAX_DELAY);
	 HAL_UART_Transmit(&huart2, (uint8_t *)time, strlen(time), HAL_MAX_DELAY);
}

This is the code I wrote.Can you pls tell where I went wrong?
 

ST Employee
June 27, 2024

Hello @AnanyaRavi29 

In Sleep mode, only certain interrupts can wake up the microcontroller, make sure that the RTC wakeup interrupt is enabled

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.