Question
st429 Disco Expansion Board
Posted on December 20, 2013 at 23:08
Hi ;)
I finally get all the material for build my little expansion board. I have now 16Mb External SDRAM and a Direct VGA output. We can use a 512k x 16Bits SRAM too but is not necessary , i think with a total of 24Mb SDRAM we can do allot ;) Actually i am cleaning my code and i will post it when finished. Everything is working very well , i use a Wii Classic controller with I2C and 2 x TM1638 with 48 Buttons in SPI :) It's just bad that the SDIO port just have the D0 pin free, i use then my SD Card in 1 bit mode. The most difficult was to remade a graphics library , the ST example is so buggy that it was unusable :( So , for more info you can take a look here :https://sites.google.com/site/suprabotics/stm429-discovery-expansion-board-v2-0
Cheers. PS : i have see a Linux port for the st429 Disco board around , i think this expansion can help with the more memory ;) #gerber-file