Skip to main content
scott239955_stm1_stmicro
Associate II
February 2, 2016
Question

ST32L476 use of VREF+

  • February 2, 2016
  • 4 replies
  • 1240 views
Posted on February 02, 2016 at 17:01

Thanks for any help. I'm confused on how to connect VREF+. I see that it can be used as an reference voltage output, and I now have it as No Connect. VDDA is connected to its pin, which seems to provide the voltage reference needed for the ADC.

So, my question: Is this enough for the ADC to work (VREF+ No Connect)? We're about to roll with boards, and I'd rather not do an ECO at this point, but I'd also rather have it work :)
    This topic has been closed for replies.

    4 replies

    waclawek.jan
    Super User
    February 2, 2016
    Posted on February 02, 2016 at 17:29

    Even if you intend to use the internal voltage reference, the datasheet requires you to connect a typ.1uF capacitor (see ''VREFBUF characteristics'').

    You should've read also AN4555.

    JW
    scott239955_stm1_stmicro
    Associate II
    February 2, 2016
    Posted on February 02, 2016 at 18:39

    Thanks JW.

    And if I want to use VDDA as the reference voltage (and not use the internal), do you think I can just tie VREF+ to VDDA? What would the consequences be -- some potential noise on VREF? Pardon my ignorance, this is my first foray into digital. 

    Cheers,

    Scott

    waclawek.jan
    Super User
    February 2, 2016
    Posted on February 02, 2016 at 22:40

    > And if I want to use VDDA as the reference voltage (and not use the internal), do you think I can just tie VREF+ to VDDA?

    Of course you can - it's what ST does on smaller packages, anyway, inside the package.

    > What would the consequences be -- some potential noise on VREF?

    Noise and fluctuations (which at the end of the day is the same, at different frequencies). Absolute precision can be checked/compensated using the internal reference.

    VDDA does not source heavy logic - that's what VDD is for - so it may be almost as good as a separate external reference, if VDDA is properly designed for. Don't forget about quite grounds, too, especially VSSA. Have you consulted that appnote?

    Also be prepared for quite a significant noise in the ADC itself. Read thoroughly the values given in the datasheet, these add up to the proportion of VREF noise.

    > Pardon my ignorance, this is my first foray into digital.

    But, isn't ADC as analog as it gets, in the realm of microcontrollers? ;)

    Jan

    scott239955_stm1_stmicro
    Associate II
    February 5, 2016
    Posted on February 05, 2016 at 22:15

    Funny!

    Thanks for the help Jan.