Skip to main content
alexanders.farley9
Associate II
December 12, 2012
Question

ST-LINKV2 + 20-10 pin, STM32F4 ''target not connected''

  • December 12, 2012
  • 2 replies
  • 805 views
Posted on December 12, 2012 at 22:34

I'm trying to program an STM32F415VG on a new board design. The board has power (3.3V) and the connectivity appears to be correct from the 10-pin Cortex Debug header to the chip although I'm doublechecking right now. The BOOT0 pin is pulled high on the board. 

Both IAR Embedded Workbench and ST-LINK utilities say no target connected. 

Are there any simple checks I can do? The chip shouldn't need anything other than power, correct SWD connectivity and BOOT0 high right? *Edit* just tested with BOOT0 pulled low, same result. 
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    December 12, 2012
    Posted on December 12, 2012 at 23:03

    With BOOT0 High you can ping USART1 or USART3 for signs-of-life

    Send 0x7F at 9600 8E1, and see if you get an 0x79 response.

    Generally check the Analogue and Digital supplies, NRESET/NRST level.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    alexanders.farley9
    Associate II
    December 13, 2012
    Posted on December 13, 2012 at 17:11

    Turns out the header pinout was wrong... the 10-pin footprint used ''IC'' style numbering (counterclockwise) instead of raster. Thanks for the help.