Question
ST-LINK/V2 vs stm32f4discovery?
Posted on September 13, 2014 at 01:46
I am having troubles setting up IAR Function Profiler so I wanted to double-check:
The grey ''ST-LINK/V2'' device vs the debug interface within discovery board. Are these the same exact thing? At least my Windows displays both as STlink dongle. I have ''normal'' breakpoints working with IAR debugger but I cannot figure out how to get Function Profiler functioning. The UI there is... special. What CPU clock does SWO configuration window refer to - is that 168MHz in my case or is if the CPU clock of the debugger? Would it be the default 72MHz? What else can I be missing?