Skip to main content
opgbartolovic
Associate
August 11, 2016
Question

ST-LINK Utility external NOR-FLASH programming

  • August 11, 2016
  • 10 replies
  • 2342 views
Posted on August 11, 2016 at 12:18

Hello

.

I have ARM MCU board

STM32F407

(Schematic: http://www.keil.com/mcbstm32f200/mcbstm32f200-schematics.pdf )

It is connected to

NOR FLASH ( http://www.jameco.com/Jameco/Products/ProdDS/1472780.pdf ) who want

to program

in ST

-Link

Utility.

I have a problem with writing * .stldr for ST

LINK.

Please help with configuring ''

Dev_Info.c

''

Is this configuration

good

:

struct StorageInfo const StorageInfo  =

 {

   ''KEIL_BOARD'',          

   NOR_FLASH,                                          

   0x60000000,                                       

   0x00400000,                                        

   0x00000002,                                      

   0xFF,                                              

// Specify Size and Address of Sectors (view example below)

    0x00000008, 0x00001000,           

    0x0000007F, 0x00008000,        

    0x00000000, 0x00000000,         

}; 

#stm32 #external-memory #nor-flash
    This topic has been closed for replies.

    10 replies

    opgbartolovic
    Associate
    August 15, 2016
    Posted on August 15, 2016 at 19:24

    Does anyone wrote code for programming the external memory for ST-Link

    ?

    Tesla DeLorean
    Guru
    August 15, 2016
    Posted on August 15, 2016 at 20:47

    Does anyone wrote code for programming the external memory for ST-Link?

    Yes, are you in the market for such?

    Your data structure really doesn't seem to accurately describe the M29W640FT NOR memory. Did you review the cited data sheet?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    opgbartolovic
    Associate
    August 15, 2016
    Posted on August 15, 2016 at 21:41

    A more detailed

    description of the structure

    :

    struct StorageInfo const StorageInfo  =  {

       ''KEIL_BOARD,V1.0'',                   // Device Name + version number

       NOR_FLASH,                               // Device Type

       0x60000000,                                  // Device Start Address

       0x00400000,                                  // Device Size in Bytes (16MBytes/128Mbits)

       0x00000008,                                  // Programming Page Size 16Bytes

       0xFF,                                             // Initial Content of Erased Memory

    // Specify Size and Address of Sectors

        0x00000008, 0x00001000,            // 8 Sectors of 8KBytes        

        0x0000007F, 0x00008000,            // 127 Sector of 64KBytes    

        0x00000000, 0x00000000,            // End

    }; 

    Tesla DeLorean
    Guru
    August 15, 2016
    Posted on August 15, 2016 at 22:34

    Half the numbers and comments are wrong.

    Your FSMC initialization would also need to be 100% correct to stand any chance of working.

    I would suggest you code NOR Writing into your current application/template, and prove and test that outside of the ST framework. Once you have that working properly you'll be in a position to port it into the loader format.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    opgbartolovic
    Associate
    August 16, 2016
    Posted on August 16, 2016 at 07:31

    Can you help with structure?

    FSMC configuration is correct. Communication memory is tested. Tested function FSMC_NOR_Test(void), gives correct results

    void BOARD_NOR_Init(void)
    { 
    FSMC_NORSRAM_TimingTypeDef NorTiming;
    FSMC_NORSRAM_InitTypeDef NorInit;
    NorInit.NSBank = FSMC_NORSRAM_BANK1;
    NorInit.DataAddressMux = FSMC_DATA_ADDRESS_MUX_DISABLE;
    NorInit.MemoryType = FSMC_MEMORY_TYPE_NOR;
    NorInit.MemoryDataWidth = FSMC_NORSRAM_MEM_BUS_WIDTH_16;
    NorInit.BurstAccessMode = FSMC_BURST_ACCESS_MODE_DISABLE;
    NorInit.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_LOW;
    NorInit.WrapMode = FSMC_WRAP_MODE_DISABLE;
    NorInit.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS;
    NorInit.WriteOperation = FSMC_WRITE_OPERATION_ENABLE;
    NorInit.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE;
    NorInit.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE;
    NorInit.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_DISABLE;
    NorInit.WriteBurst = FSMC_WRITE_BURST_DISABLE;
    /* Timing */
    NorTiming.AddressSetupTime = 6;
    NorTiming.AddressHoldTime = 15;
    NorTiming.DataSetupTime = 6;
    NorTiming.BusTurnAroundDuration = 15;
    NorTiming.CLKDivision = 2;
    NorTiming.DataLatency = 17;
    NorTiming.AccessMode = FSMC_ACCESS_MODE_B;
    /* Initialize NOR control Interface */
    FMC_NORSRAM_Init(FSMC_NORSRAM_DEVICE, &NorInit);
    /* Initialize NOR timing Interface */
    FMC_NORSRAM_Timing_Init(FSMC_NORSRAM_DEVICE, &NorTiming, NorInit.NSBank);
    /* Initialize NOR extended mode timing Interface */
    FMC_NORSRAM_Extended_Timing_Init(FSMC_NORSRAM_EXTENDED_DEVICE, &NorTiming, NorInit.NSBank, NorInit.ExtendedMode);
    /* Enable the NORSRAM device */
    __FMC_NORSRAM_ENABLE(FSMC_NORSRAM_DEVICE, NorInit.NSBank);
    /* SRAM controller initialization */
    BOARD_GPIO_NOR_Init();
    }
    void FSMC_NOR_Test(void)
    {
    uint16_t index;
    HAL_NOR_StatusTypeDef flag_erase = HAL_NOR_STATUS_ERROR;
    flag_erase = FSMC_NOR_EraseChip();
    FSMC_NOR_EraseBlock(WRITE_READ_ADDR);
    for (index = 0; index < BUFFER_SIZEE; index++ )
    {
    TxBuffer[index] = index + 121;
    }
    FSMC_NOR_WriteBuffer(TxBuffer, WRITE_READ_ADDR, BUFFER_SIZEE);
    /* Read data from FSMC NOR memory */
    FSMC_NOR_ReadBuffer(RxBuffer, WRITE_READ_ADDR, BUFFER_SIZEE);
    if( memcmp( (char*)TxBuffer, (char*)RxBuffer, BUFFER_SIZEE ) == 0 )
    {
    HAL_GPIO_WritePin(LED6_GPIO_PORT,LED6_PIN, GPIO_PIN_SET); // Nor Flash is OK
    }
    else
    {
    HAL_GPIO_WritePin(LED6_GPIO_PORT,LED6_PIN, GPIO_PIN_RESET); // Nor Flash is error
    }
    }

    opgbartolovic
    Associate
    August 17, 2016
    Posted on August 17, 2016 at 12:23

    I'm still

    double-check

    code.

    Code is

    well written.

    The structure is not good?

    What's wrong?

    Tesla DeLorean
    Guru
    August 17, 2016
    Posted on August 17, 2016 at 14:19

    The structure is not good? What's wrong?

    Like I told you, half the numbers are wrong, this should correctly describe the part

    struct StorageInfo const StorageInfo = {
    ''KEIL_MCBSTM32F400_M29W640FT/V100'', // Device Name + version number
    NOR_FLASH, // Device Type
    0x60000000, // Device Start Address
    0x00800000, // Device Size in Bytes (8MBytes/64Mbits)
    0x00000008, // Programming Page Size 8Bytes (Nominal)
    0xFF, // Initial Content of Erased Memory
    // Specify Size and Address of Sectors
    0x00000008, 0x00002000, // 8 Sectors of 8KBytes 
    0x0000007F, 0x00010000, // 127 Sector of 64KBytes 
    0x00000000, 0x00000000, // End
    }; 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    opgbartolovic
    Associate
    August 17, 2016
    Posted on August 17, 2016 at 14:54

    Can a more detailed

    description of the structure

    ?

    Board MCBSTM32F400

    have M29W640FB (not M29W640FT )

    0x60000000

    - start address is correct

    0x00800000

    - memory pin 47 (BYTE#),

    connected to

    VCC,

    then

    - data 16bit - memory size 4Mb ???

    0x00000008 - Programming Page, good size pages ???  

    Tesla DeLorean
    Guru
    August 17, 2016
    Posted on August 17, 2016 at 15:29

    It is a 64Mb device whether it is accessed as bytes or words. There are 8MB in a 64Mb device. The CPU has a byte addressable address space, and these bytes don't change size if the downstream bus needs to handle 8, 16 or 32-bit widths to the memory array.

    Mb megabit

    MB megabyte

    8x1024x1024 = 8388608 = 0x800000

    4096 = 0x1000

    8192 = 0x2000

    65536 = 0x10000

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    August 17, 2016
    Posted on August 17, 2016 at 15:38

    Board MCBSTM32F400

    have M29W640FB (not M29W640FT )

     

    Not my board, adjust the string as desired.

    ''KEIL_MCBSTM32F400_M29W640FB70N6E/V100'',          // Device Name + version number

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..