Skip to main content
manishbaing2789
Associate III
July 22, 2013
Question

st-link for stm32f3discovery

Posted on July 22, 2013 at 11:49

Hello I am facing problem to download st-link/v2 for stm32f3 discovery for linux.plz guide me or give me some links realted to that.

    This topic has been closed for replies.

    5 replies

    crt2
    Visitor II
    July 22, 2013
    Posted on July 22, 2013 at 14:39

    What kind of problem and why would you need st-link for? If you're on linux openocd+gdb+gcc should be something to consider...

    manishbaing2789
    Associate III
    July 24, 2013
    Posted on July 24, 2013 at 10:37

    thanks for reply but now i have download it from

    https://github.com/texane/stlink

    crt2
    Visitor II
    July 24, 2013
    Posted on July 24, 2013 at 10:50

    Dont open multiple threads - you will create confusion.

    I do not think there is indication that program is halted at all. Now I wonder why would you think so, and I wonder what is in line 39 in main.c

    Maybe send ''monitor reset init'' instead of just ''monitor reset''

    manishbaing2789
    Associate III
    July 24, 2013
    Posted on July 24, 2013 at 11:08

    Sorry for Creating multiple threads.Fact is that  I am new to this forum and I didn't get how to post and post is posted correctly or not.but now I got it and I will take care of now-onwards.

    manishbaing2789
    Associate III
    July 24, 2013
    Posted on July 24, 2013 at 11:18

    I have send ''monitor reset init'' instead of  ''monitor reset'' but till same problem.

    I am trying to debug software timer using freeRTOS. main.c mentioned below .

    But I feel  that it  may not problem of any source file.beacause I have check with LED blink code also but same problem so.

    main.c

    /*! header files */

    #include ''stm32f4xx.h''

    #include ''FreeRTOS.h''

    #include ''timers.h''

    #include <math.h>

    #include <stdio.h>

    #include <stdlib.h>

    typedef void * xTimerHandle;

      /*! Timer Expirecounter   */

      long lExpireCounters = 0 ;          

       /*!  Handle to xtimerAPIs  */

       xTimerHandle xTimer;

     

      /*!

       * callback function

       *  count the number of times the

       * associated timer expires, and stop the timer once the timer has expired

       * 10 times.

       */

      void vTimerCallback( xTimerHandle pxTimer )

      {

        

          const long MaxExpiryCount = 10 ;               /*! Maximum Expiry ount */

          

     

              /*! Increment the number of times that Timer has expired. */

              lExpireCounters += 1;

     

              /*! If the timer has expired 10 times then stop it from running.*/

              if( lExpireCounters == MaxExpiryCount )

              {

              xTimerStop( pxTimer, 0 );                     /*! Timer Stop if Condition satisfied */

              }

      }

     

         int main( void )

        {

                long x=1;

    // line no 39

               /*! Create timer */

               xTimer = xTimerCreate(  ''Timer''      ,         /*! Name for timer */

                                       (100)        ,            /*! The timer period in ticks.(1 ticks = 1ms) */

                                        pdTRUE      ,         /*! The timers will auto-reload themselves when they expire. */

                                        (void *) x   ,        /*! timer a unique id */

                                        vTimerCallback        /*! callback fuction ,called when Timer get expires */

                                    );

     

               if( xTimer == NULL )

               {

                 printf(''Timer not created'');

                   /*!  The timer was not created. */

               }

               else

               {

                   /*! Start the timer. */

                   if( xTimerStart ( xTimer, 0 ) != pdPASS )

                   {

                       /* The timer could not be set into the Active state.*/

                   }

     

                  else

                   {

                      printf(''Timer start sucessfully\n'');

                   }

               }

          

            /*! Task scheduling started */    

            vTaskStartScheduler();

          

           while (1);

     }