Skip to main content
micha
Associate
August 9, 2010
Question

ST-LINK Commandline Tool

  • August 9, 2010
  • 3 replies
  • 922 views
Posted on August 09, 2010 at 08:41

ST-LINK Commandline Tool

    This topic has been closed for replies.

    3 replies

    LaurentL
    ST Employee
    May 17, 2011
    Posted on May 17, 2011 at 14:01

    Hello,

    First, there is an issue in the protocol in your command line, on STM32, you should use JTAG or SWD, not SWIM (only for STM8).

    I suppose it is a copy paste issue. ;)

    For your programming issue, there has been a correction in latest version of STVP (ST Visual Programmer).

    Download the latest ST toolset with latest STVP version (3.2.1), it should work.

    Another workaround is to recopy the APISample.exe and your 2 hex file in STVP directory.

    If you still have the issue, your flash is not virgin.

    If you want to reprogram a device, i suggest you add the ''-erase'' command.

    I just tried this twice, it is working fine:

    APISample.exe -BoardName=ST-LINK -Device=STM32F103xB -Port=USB -ProgMode=SWD -no_loop -no_log -FileProg=STM32F103xB_prog.hex -FileOption=STM32F103_option.hex -erase

    Here is the result:

    Configuration:

    BoardName=ST-LINK Device=STM32F103xB Port=USB ProgMode=SWD

    >>> Loading file STM32F103xB_prog.hex in PROGRAM MEMORY

    >>> Loading file STM32F103_option.hex in OPTION BYTE

    >>> Erasing PROGRAM MEMORY

    (API) WARNING :   Mass Erasing device...

    (API) WARNING :   Blank Checking device...

    <<< Erasing PROGRAM MEMORY succeeds

    >>> Programming PROGRAM MEMORY

    <<< Programming PROGRAM MEMORY succeeds

    >>> Verifying PROGRAM MEMORY

    <<< Verifying PROGRAM MEMORY succeeds

    >>> Programming OPTION BYTE

    <<< Programming OPTION BYTE succeeds

    >>> Verifying OPTION BYTE

    <<< Verify OPTION BYTE succeeds

    Regards,

    Laurent

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    pwootton
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 14:01

    Is there anyway to reset and run the device with this API?

    micha
    michaAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 14:01

    Ok,

    it works with the new toolkit.

    Thank you

    Regards

    Mike