Skip to main content
xiaowei zhang
Visitor II
July 4, 2018
Question

st-link CLI to download data to on chip sram without reset the chip.

  • July 4, 2018
  • 0 replies
  • 413 views
Posted on July 04, 2018 at 02:05

Hi,

I uses ST-LINK CLI command '-P <file> 0x20000000' to load data file to sram. When the load is

finished, the MCU is also

rested.

It is possible to use st-link CLI to download the data to 

the

 on chip sram without reset the chip.

    This topic has been closed for replies.