Skip to main content
Associate
Mar 11, 2024 8:08 AM UTC
Solved

ST bootloader - pin states

Hi,

I'm currently gaining experience with the STM32G4, whose ROM bootloader supports various interfaces. AN2606 describes the configuration of the pins occupied by the interfaces.
Various pins are operated in push-pull mode, which can lead to undesirable effects in an external circuit.
My question is whether it is possible to deactivate unneeded interfaces in the bootloader, e.g. via option bytes, or whether this can only be achieved with a separate bootloader.

Thanks in advance for your feedback!

This topic has been closed for replies.
TDK
TDKBest answer
Mar 11, 2024 1:21 PM UTC

> My question is whether it is possible to deactivate unneeded interfaces in the bootloader, e.g. via option bytes, or whether this can only be achieved with a separate bootloader.

No, it is not possible to change the behavior of the bootloader in any way. You cannot disable interfaces selectively.

However, most pins are in input mode and it is only a problem if they are being toggled externally, which could be misinterpreted as activity on that bus.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

AlexSmart
Associate III
Mar 11, 2024 8:15 AM UTC

Sure, there is a special option bit for it called nSWBOOT0

AlexSmart_0-1710144916777.png

 

kf_SEAAuthor
Associate
Mar 11, 2024 8:40 AM UTC

Hi @AlexSmart 

thanks, but the question not about the pins or option bytes to enter the bootloader but about the interfaces supported by the bootloader for communication (USART, SPI, IC2). For all of them the bootloader configures GPIOs (AN2606) which can conflict with the external circuit. I'm interested if some of these interfaces can be disabled for the bootloader.

kr

TDK
TDKBest answer
Mar 11, 2024 1:21 PM UTC

> My question is whether it is possible to deactivate unneeded interfaces in the bootloader, e.g. via option bytes, or whether this can only be achieved with a separate bootloader.

No, it is not possible to change the behavior of the bootloader in any way. You cannot disable interfaces selectively.

However, most pins are in input mode and it is only a problem if they are being toggled externally, which could be misinterpreted as activity on that bus.

"If you feel a post has answered your question, please click ""Accept as Solution""."