Skip to main content
woutervddn
Visitor II
November 12, 2010
Question

ST, all but userfriendly

  • November 12, 2010
  • 10 replies
  • 2394 views
Posted on November 12, 2010 at 18:30

hi all,

first of, I just got my STM32VL Discovery. And it looks nice!

I took it out, pluged it in and an played with the buttons..

NICE!

Next step: (5 on the cardboard btw)

to study or modify the DISCOVER project related to this simple demo,

visit www.st.com/stm32-discovery and follow the tutorial.

Nice try but a 404 is given..

After some google search I decided to download Atollic.

I find the st tutorial and think I'm all set.

Guess again.. the tutorial says I have to go to the stm32vl_discovery directory..

But I can't find it (how could I, I didn't even downloaded something from st).

Anyways, my google search starts again, and by wonder I stumble upon the an3268 package. I hate to say it, but this is sh*t, how could I knew this? I never, ever found a download location. I didn't even got the hint that I had to download something..

But I'm set, atleast I think..

in the next step I need to add a variable path.. It points to a FIRMWARE folder,.. NICE, but where the hell is it located? I couldn't find it, so I suppose it's another download link... 

But where in earth can I find it? One thing is certain, NOT in the tutorial..

Wouter Vandenneucker

PS: can someone pls give me that link.. it's kind of frustrating..

#firmware #stm32vl #package #tutorial
    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    November 12, 2010
    Posted on November 12, 2010 at 23:45

    The site is in transition

    Here is the new discovery page, files under Design Support tab

    http://www.st.com/internet/evalboard/product/250863.jsp

    http://www.st.com/internet/evalboard/product/250863.jsp

    Firmware source/libraries

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3268.zip

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3268.zip

    These need to be unzipped in a suitable place, with Keil under Examples\ST worked for me.

    I wouldn't touch Atollic Lite, it doesn't support project files, and building stuff for the VL board was a battle. Keil was easier, but embedded stuff generally assumes you can use, or are familiar, with the tools.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    November 13, 2010
    Posted on November 13, 2010 at 08:04

    ''The site is in transition''

    From something that was usable to something that is not!

    :(

    Note that the 

    http://www.st.com/stm32-discovery

    URL has now been fixed.

    But I'm sure you'll not be the only one to be seriously frustrated by this gross stupidity on ST's part! Especially as it coincides with the launch of two design contests (that I know of)!!

    See the following thread for discussion about the dreadful new website: 

    [DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Website%20Wrecked%21&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General comments and feedback/Website Wrecked!&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    alwebbox
    Visitor II
    November 16, 2010
    Posted on November 16, 2010 at 07:17

    Andrew Neil
    Super User
    November 16, 2010
    Posted on November 16, 2010 at 09:13

    ''I wouldn't touch Atollic Lite, it doesn't support project files''

     

    It also completely prevents you from using printf!

    That's not just that it doesn't come with a complete implementation, so you have to write your own - they have specifically disabled the facilities needed to allow you to use it at all!!

    ''I selected the Atollic option based on the fact that it has no code size restrictions and therefore seemed to be the most capable''

    See above!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    November 16, 2010
    Posted on November 16, 2010 at 21:56

    (deleted by me)

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    alwebbox
    Visitor II
    November 17, 2010
    Posted on November 17, 2010 at 04:48

    ''It also completely prevents you from using printf!''

     

     

    Maybe that's what they mean in the feature comparison guide?

    I/O redirection of runtime library - not in Lite version
    Andrew Neil
    Super User
    November 17, 2010
    Posted on November 17, 2010 at 08:02

    ''It also completely prevents you from using printf!''

     

     

    Maybe that's what they mean in the feature comparison guide?

     

    I/O redirection of runtime library - not in Lite version

     

     

    Yes - I think so.
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    qili
    Visitor II
    November 20, 2010
    Posted on November 20, 2010 at 12:50

    I have to say that my first impression with the redesigned st.com site that it must have been designed by nxp or one of st's competitors.

    it is so bad and so hard to use that there is no other explanation.

    Andrew Neil
    Super User
    November 20, 2010
    Posted on November 20, 2010 at 20:32

    Please keep comments about the new website in the specific thread about it:

    [DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Website%20Wrecked%21&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0&currentviews=292]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Website%20Wrecked!&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0&currentviews=292

    That way ST can see all the posts together - rather than have them ''hidden'' in other threads.
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    noelbautista
    Visitor II
    December 3, 2010
    Posted on December 03, 2010 at 11:31

    I have the same experience.  I really hate it when these documents that are supposed to help you get started isn't doing its job.

    I guess some tech guys are doing the documentation which in my experience, most tech guys aren't really good at such a job.  Normally, tech guys hate doing documentation work.  

    They must have a good technical documentation person.  Morever, even the tool chain softwares aren't properly documented either.  What you see in the quickstart guides isn't what you'll see when you actually do it and download their softwares.  If they will upgrade or change their softwares, they must always update their manuals, docs, and guides.