Skip to main content
NJP.1
Associate III
September 27, 2021
Question

ssd1327 oled display interfacing with stm32

  • September 27, 2021
  • 1 reply
  • 1332 views

Hi have been working on the interfacing of ssd1327 with stm32 microcontroller, i am just trying to print a pixel on the display but I could not display it. my code is as follows

WRITECOMMAND(0xae);

 //

 WRITECOMMAND(0x15);

 WRITECOMMAND(0x00);

 WRITECOMMAND(0x7f);

WRITECOMMAND(0x75);

 WRITECOMMAND(0x00);

 WRITECOMMAND(0x7f);

 WRITECOMMAND(0x81);

 WRITECOMMAND(225);// this is for contrast

 WRITECOMMAND(0xa0);

 WRITECOMMAND(0x51);

 WRITECOMMAND(0xa1);

 WRITECOMMAND(0x00);

WRITECOMMAND(0xa2);

 WRITECOMMAND(0x00);

 // SSD1306_WRITECOMMAND(0xa6); //this is for on all the pixels a6 to off all the pixels

 WRITECOMMAND(0xa8); //set multiplex ratio

 WRITECOMMAND(0x7f);

 WRITECOMMAND(0xab); //set multiplex ratio

 WRITECOMMAND(0x01);

 WRITECOMMAND(0xb6); //set phase leghth

 WRITECOMMAND(0x0f);

 WRITECOMMAND(0xbe); //Set vcomh voltage

 WRITECOMMAND(0x0f);

 WRITECOMMAND(0xbc); //set pre-charge voltage

 WRITECOMMAND(0x08);

 WRITECOMMAND(0xd5); //second precharge period

 WRITECOMMAND(0x62);

 WRITECOMMAND(0xfd); //Unlock commands

 WRITECOMMAND(0x12);

 WRITECOMMAND(0xaf);

 HAL_Delay(1500);

 // SSD1306_WRITECOMMAND(0xa5);

 // SSD1306_WRITECOMMAND(0xa6);

 WRITECOMMAND(0x15);       /* Set Column Address */

 WRITECOMMAND(0x08); /* Start Column: Start from 8 */

WRITECOMMAND(0x37);       /* End Column */

   // Row Address

 WRITECOMMAND(0x75);       /* Set Row Address */

 WRITECOMMAND(0x08);   /* Start Row*/

 WRITECOMMAND(0x37);   /* End Row*/

 HAL_Delay(100);

   WRITEDATA(0x01);

#define WRITECOMMAND(command)   ssd1306_I2C_Write(SSD1306_I2C_ADDR, 0x00, (command))

/* Write data */

#define WRITEDATA(data)      ssd1306_I2C_Write(SSD1306_I2C_ADDR, 0x40, (data))

This topic has been closed for replies.

1 reply

TDK
September 28, 2021

Can you see the I2C signals on the board? Does the controller ACK?

Do these commands match up to some known good working initialization that you found somewhere, preferably in the datasheet?

"If you feel a post has answered your question, please click ""Accept as Solution""."