Skip to main content
TARHAN SAMAH
Senior
Nov 7, 2017 8:24 AM UTC
Solved

spirit 1 , and stm32f103xx?

Posted on November 07, 2017 at 09:24

Hello every body we are using stm32f103xx microcontrollers , we want to send our data by wireless using spirit1 module ,

- is it possible ?

-which library is suitable ?

-what about distance amd range of gigahertz modules ?

urgent help needed plz thanks 

Samah Tarhan 

Argebilisim 

    This topic has been closed for replies.
    TARHAN SAMAH
    TARHAN SAMAHBest answer
    Senior
    Nov 16, 2017 11:27 AM UTC
    Posted on November 16, 2017 at 12:27

    İ SOLVE it it was a wrong adapter from hyperterminal to ttl , before i used adm now i use usb dongle ch340g or arduino adapter . now i communicate perfectly with my spirit 1 ,thanks 

    14 replies

    Andrew Neil
    Super User
    Nov 7, 2017 9:17 AM UTC
    Posted on November 07, 2017 at 10:17

    Surely, the answer to this will be found by reading the documentation for this '

    spirit1 module'?

    You have done that, haven't you ... ?

    http://www.8052.com/forum/read/160143

     (it's not by any means new - but it is certainly still applicable!)
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Nov 7, 2017 10:22 AM UTC
    Posted on November 07, 2017 at 10:22

    Ah - you mean this: 

    http://www.st.com/en/wireless-connectivity/spirit1.html

     

    Loads of documents on that page for you to read!

    Just looking at the very first paragraph of the Dev Kit User Manual:

    The kit includes a SPIRIT1 development kit graphical user interface (SPIRIT1 DK - GUI) which allows checking the SPIRIT1 main performance and easily measure parameters such as sensitivity, output power and main features of the SPIRIT1. It also

    contains SPIRIT1 firmware libraries for STM32L

    and STM8L to allow development of SPIRIT1 applications.
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    TARHAN SAMAH
    Senior
    Nov 7, 2017 10:40 AM UTC
    Posted on November 07, 2017 at 10:40

    thanks so much mister Andrew ,, so it will not be possible to use on my stm32f103xx series maybe from another libraries  ? , 

    -what about transmition range ?? 

    also i got another question if we use the STM32ML and wmbus is it free standart or needs fees ? 

    Tesla DeLorean
    Guru
    Nov 7, 2017 4:27 PM UTC
    Posted on November 07, 2017 at 17:27

    Everything you post to the forum is 'urgent', please read the Hacker FAQ to understand how such requests are interpreted. 

    http://www.catb.org/esr/faqs/smart-questions.html#urgent

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    TARHAN SAMAH
    Senior
    Nov 14, 2017 2:44 PM UTC
    Posted on November 14, 2017 at 14:44

    thanks  to all of you ok now i see better , we need to make it in two steps first send the firmware to the sp1ml via st link2 then use the uart in application mode like wireless uart ,,, i was really lost , im beginner ,, didnt know that urgent had a haker meaning , just my request was really huamnly urgent )) ..the support team of st helped me to see clearer .. thanks

    Andrew Neil
    Super User
    Nov 14, 2017 4:03 PM UTC
    Posted on November 14, 2017 at 17:03

    doumandjisamah wrote:

    Argebilisim 

    Is that this '

    Argebilisim': 

    http://www.argebilisim.com/en/index.html

     
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    TARHAN SAMAH
    Senior
    Nov 15, 2017 2:58 PM UTC
    Posted on November 15, 2017 at 14:58

    YES İT İS we are in Istanbul, 

    TARHAN SAMAH
    Senior
    Nov 15, 2017 2:19 PM UTC
    Posted on November 15, 2017 at 15:19

    ok now i got the firmware and download the binary to the sp1ml using st-link , looks it is downloaded , now i want to test the AT COMMAND mode using the hyperterminal , first let me tell you the hardware connections pins :

    -SHDN  connected to 3,3v , always power up 

    -mode0 to 0, it is command mode

    -vdd 3,3v 

    -gnd to gnd 

    -rx of spirit to tx of hyperterminal 

    -tx of spirit to rx of hyperterminal 

    -reset to button 3,3v to 0volts

    i use baudrate 9600 and CR after sending :

    ,  i opened hyperterminal after reset i got '?',   so i entererd to command mode '+++' no answer , i tried AT nthg comes from spirit,??? is there something i missed 

    TARHAN SAMAH
    TARHAN SAMAHAuthorBest answer
    Senior
    Nov 16, 2017 11:27 AM UTC
    Posted on November 16, 2017 at 12:27

    İ SOLVE it it was a wrong adapter from hyperterminal to ttl , before i used adm now i use usb dongle ch340g or arduino adapter . now i communicate perfectly with my spirit 1 ,thanks