Skip to main content
miroslav
Associate II
January 27, 2014
Question

SPI3 problem with STM32f4- discovery and stm32f103

  • January 27, 2014
  • 7 replies
  • 1741 views
Posted on January 27, 2014 at 13:42

Hi,

I have problem with SPI3 and st-link debugger. CLK pin is always unaveilable.

I configure MCU to not use JTDO but in debug mode when I look at AFIO register there is written some other value for SWJ_CFG(always 0x50) and I want it to be 0x20.

I already work with SPI1 and SPI2 and they work perfect in interrupt and non-interrupt mode.

How to solve problem?

there is little code:

tmp = AFIO->MAPR;

tmp &= 0xF8FFFFFF;

tmp |= AFIO_MAPR_SWJ_CFG_JTAGDISABLE;

AFIO->MAPR = tmp;

  DBGMCU->CR &= ~DBGMCU_CR_TRACE_IOEN; //disable async trace for every case

it works same as GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE); 

All the best,

Miroslav

#stm32 #stm32-st-link-swd #stm32discovery
    This topic has been closed for replies.

    7 replies

    miroslav
    miroslavAuthor
    Associate II
    January 27, 2014
    Posted on January 27, 2014 at 13:47

    Hi,

    Also PB3 pin, used for CLK I can't use for anything as I can't even toggle it like GPIO.

    Here are port settings:

    GPIO_InitStructure.GPIO_Pin = CLK | MOSI ;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    waclawek.jan
    Super User
    January 27, 2014
    Posted on January 27, 2014 at 14:09

    > Subject: SPI3 problem with STM32f4 an stm32f103

    So is it STM32F4, or STM32F103?

    > I configure MCU to not use JTDO but in debug mode when I look at AFIO register there is

    > written some other value for SWJ_CFG(always 0x50) and I want it to be 0x20.

    Isn't SWJ_CFG a 3-bit bitfield? Then it can't be 0x50 nor 0x20.

    AFIO clock enabled when you try to rewrite its registers?

    > Also PB3 pin, used for CLK I can't use for anything as I can't even toggle it like GPIO.

    Once you set it to AF, then you can't use it as a GPIO output.

    JW

    miroslav
    miroslavAuthor
    Associate II
    January 27, 2014
    Posted on January 27, 2014 at 14:23

    Hi,

    I use STM32F03 with st-link debbuger.

    It imposible to set AFIO register.

    Every value written will always be restored by debugger.

    miroslav
    miroslavAuthor
    Associate II
    January 27, 2014
    Posted on January 27, 2014 at 14:31

    As i said, when I set it to be GPIO out, not AF, I can't use it. 

    Next line:

     AFIO->MAPR = ''what ever I put''; will resul that MAPR is 0x04000000.

    That is also lie!!! Because 0x04000000 will disable JTAG and SW together but debugger continue working!

    waclawek.jan
    Super User
    January 27, 2014
    Posted on January 27, 2014 at 15:04

    AFAIK, STLink is a relatively dumb USB-to-JTAG/SWD convertor.

    So, if you suspect ''something'' is overwriting the registers during debugging, it's the PC-side software you have to blame. You might want to review the documentation coming with that.

    JW

    miroslav
    miroslavAuthor
    Associate II
    January 27, 2014
    Posted on January 27, 2014 at 15:16

    Hi,

    Yes, it must be problem with ukeil. Compiler probably predefine some settings for that.

    Funny thing is that on ukeil without debbuger selected, built code after UART download works!

    Once I select debugger all stop working and I cant return to previous state.

    All the best,

    Miroslav

    miroslav
    miroslavAuthor
    Associate II
    January 27, 2014
    Posted on January 27, 2014 at 17:03

    All working now,

    One global chip erase did the job.

    All the best and thanx for atention.

    Miroslav