Question
spi transmit without mcu control
Posted on January 20, 2017 at 06:22
I'm learing stm32 spi,
In normal way of master mode,
I have to low the slave select pin, then transmit data, then high the slave select pin
I know that I can use dma to transmit data,
but I am not sure that dma can control slave select pin or not?
Can I have anyway to to whole transmit data(including control slave select pin) using all hardware?
#dma #stm32 #spi