Question
SPI Sends Dummy bytes
Posted on March 05, 2013 at 14:32
Hello All,
I am using STM32F207VC. I have problem while sending data to slaves. I send a packet of data for example 0x01,0x02,0x03,0x04,0x05,0x06. While sending these packets SPI sends 0x00 in between anyof these data and my actual data is skipped.So My Slave doesnt understand what I am sending and its not responding. Could any one pls let me know what could be the problem. I am stuck with this since last 2 days. Here is my codeuint8_t SPIWrite(uint8_t *pBufferPtr, uint8_t ucSPIPacketLength)
{uint8_t ucCount;
uint8_t ucDummyRead; /*Assert the CS Pin to Low for SPI Slave*/ CS_LOW(GPIOB,GPIO_Pin_12); Delayus(100); for (ucCount=0; ucCount < ucSPIPacketLength; ucCount++) { while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) != SET); SPI_I2S_SendData(SPI2,*pBufferPtr ); if(SPI2->DR != *pBufferPtr) { SPI_I2S_SendData(SPI2,*pBufferPtr ); } ucDummyRead =SPI_I2S_ReceiveData(SPI2); /*wait for transmission to complete */ while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) != SET); Delayus(100); /*read the response from the spi rx buffer to dummy variable*/ ucDummyRead =SPI_I2S_ReceiveData(SPI2); while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == RESET) ; pBufferPtr++; } CS_HIGH(GPIOB,GPIO_Pin_12);return SUCCESS;
} #st