Question
SPI receive times out due to SPI_FLAG_RXNE not reseting in SPI_EndRxTransaction.
MCU is STM32F427. I'm using SPI3 to read from a transmit only slave. My configuration looks like this:
/* SPI3 parameter configuration*/
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_MASTER;
hspi3.Init.Direction = SPI_DIRECTION_2LINES_RXONLY;
hspi3.Init.DataSize = SPI_DATASIZE_16BIT;
hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi3.Init.NSS = SPI_NSS_SOFT;
hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi3.Init.CRCPolynomial = 10;When it comes time to read the code does the following:
- Sets CS low via gpio
- calls HAL_SPI_Receive
- Sets CS high via gpio
Stepping through the code in (2), I see the correct data received in two 8 bit reads. However, when the HAL code gets to the end of HAL_SPI_Receive, it does the following.
/* Check the end of the transaction */
if (SPI_EndRxTransaction(hspi, Timeout, tickstart) != HAL_OK)
{
hspi->ErrorCode = HAL_SPI_ERROR_FLAG;
}This sets the error code every time and the HAL_SPI_Receive call fails.
If I comment out the following code in SPI_EndRxTransaction, the read succeeds.
static HAL_StatusTypeDef SPI_EndRxTransaction(SPI_HandleTypeDef *hspi, uint32_t Timeout, uint32_t Tickstart)
{
if ((hspi->Init.Mode == SPI_MODE_MASTER) && ((hspi->Init.Direction == SPI_DIRECTION_1LINE)
|| (hspi->Init.Direction == SPI_DIRECTION_2LINES_RXONLY)))
{
/* Disable SPI peripheral */
__HAL_SPI_DISABLE(hspi);
}
/* Erratasheet: BSY bit may stay high at the end of a data transfer in Slave mode */
if (hspi->Init.Mode == SPI_MODE_MASTER)
{
if (hspi->Init.Direction != SPI_DIRECTION_2LINES_RXONLY)
{
/* Control the BSY flag */
if (SPI_WaitFlagStateUntilTimeout(hspi, SPI_FLAG_BSY, RESET, Timeout, Tickstart) != HAL_OK)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FLAG);
return HAL_TIMEOUT;
}
}
// COMMENT OUT THIS BLOCK AND THE SPI RECEIVE WORKS
// else
// {
// /* Wait the RXNE reset */
// if (SPI_WaitFlagStateUntilTimeout(hspi, SPI_FLAG_RXNE, RESET, Timeout, Tickstart) != HAL_OK)
// {
// SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FLAG);
// return HAL_TIMEOUT;
// }
// }
// END COMMENTED BLOCK
}
else
{
/* Wait the RXNE reset */
if (SPI_WaitFlagStateUntilTimeout(hspi, SPI_FLAG_RXNE, RESET, Timeout, Tickstart) != HAL_OK)
{
SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_FLAG);
return HAL_TIMEOUT;
}
}
return HAL_OK;
}Can someone please explain what I'm doing wrong? Thank You!