Skip to main content
ADIt
Associate II
March 2, 2019
Question

Spi read and write on different edge?

  • March 2, 2019
  • 1 reply
  • 782 views

Hi,

i am using stm32f103 spi read write

i have application ic connected to this MCU

is it possible to use write on rising egde and read on falling edge for spi communication?

currently i am doing both on rising edge

so, write now my write is ok but while reading the data it gives a different value

I am using bidirectional mode

thanks

This topic has been closed for replies.

1 reply

S.Ma
Principal
March 2, 2019

If using SPI 3 wires (data is either input or output), you can try to change the CPHA/CPOL when SPI is Idle (BUSY bit) before generating SCK clock to move data bits. On newer SPI IP versions such as STM32L4 or F7, you can also change the data bit length from 4 up to 16 bits and 32 bit FIFOs are integrated to smooth the transmission.