Skip to main content
Associate III
April 15, 2025
Question

SPI NSS cannot be switched in software mode

I am trying to use SPI communication with the STM32H562 (for FPGA programming purposes).

 

The reference manual states that if SPI_CFG2's SSM = 1, the NSS can be toggled High/Low by switching the SSI bit in SPI_CR1.

However, the switching of SSI is not reflected in the oscilloscope observations.

Additionally, I tried setting the NSS port as GPIO instead of SPI communication and using HAL_WritePin to configure it, but this was also not reflected.

When using the NSS port for SPI, should I set the start register bits such as SPE and CSTART?

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
April 15, 2025

@Thoufiel wrote:

The reference manual states that if SPI_CFG2's SSM = 1, the NSS can be toggled High/Low by switching the SSI bit in SPI_CR1.


No, that's not what it says:

AndrewNeil_2-1744712815506.png

 

 

 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ThoufielAuthor
Associate III
April 16, 2025

Thank you for your reply.

 

I had read that section before my initial question, and regarding the content just before the red line,

I understood it as "Slave select can be performed by setting the SSI bit."

What does "internally" mean in this context?

Andrew Neil
Super User
April 16, 2025

I guess it means something internal (so, your software?) has to do it by manipulating the SSI bit ?

Perhaps @STTwo-32 could clarify ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
April 15, 2025

In an SPI master, you can either use the NSS pin as SPI hardware-controlled, or you can configure it as GPIO.

If a slave, it should be hardware controlled.

> Additionally, I tried setting the NSS port as GPIO instead of SPI communication and using HAL_WritePin to configure it, but this was also not reflected.

Show relevant code and hardware setup. Controlling the pin as GPIO should be relatively simple exercise.

> When using the NSS port for SPI, should I set the start register bits such as SPE and CSTART?

Yes. The peripheral needs to be enabled in order for it to do anything.

"If you feel a post has answered your question, please click ""Accept as Solution""."