Question
SPI NSS?
Posted on July 13, 2018 at 18:36
Hi,
I am working on Nucleo-144 SPI. The NSS GPIO ios PA4. The only way I can have the NSS high is use
__HAL_SPI_DISABLE() function. The HAL_GPIO_WritePin() just never work.
I can see from the scope to verify it. Doesn't seems to be the right way to turn off the SPI for set NSS high.
Anyone has experience turn NSS high/low?
/**SPI1 GPIO Configuration
PA4 ------> SPI1_NSS PA5 ------> SPI1_SCK PA6 ------> SPI1_MISO PA7 ------> SPI1_MOSI */HAL_GPIO_WritePin( GPIOA, GPIO_PIN_4, GPIO_PIN_SET ); // NSS1 high
__HAL_SPI_DISABLE(m_spi);
Thx