SPI Mode for non standard sampling edges
Hi, i am currently working on a driver for a Chineese IC. The manufacturer recomends implementing SPI protocol over an FPGA, but for cost reasons we would like to use a MCU.
The SPI protocol that the chip uses has the following configuration
"Chip SPI samples SDI on the ris ing edge of SCL K and the rising edge of SCLK
outputs SDO, so the external host needs to output SDI on the falling edge of SCLK and sample SDO on the falling edge of SCLK."
We've been able to comunicate with the chip with some success, but due to sampling instant we are reading the correct output but 1 bit to the left.
Is there any way to configure this sampling description besides changing CPOL CPHAS configuration in the middle of the SPI transaction?
This is our reading function right now:
HAL_SPICLK_TO_GPIO(chip);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_TO_SPICLK(chip);
//SPI Read Command
HAL_GPIO_WritePin(chip->cs.bench, chip->cs.pin, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(chip->hspi, data,3, XPHASED_SPI_TIMEOUT);
HAL_GPIO_WritePin(chip->cs.bench, chip->cs.pin, GPIO_PIN_SET);
if(ret != HAL_OK){
return 1;
}
//Additional Clock Cycles
HAL_SPICLK_TO_GPIO(chip);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_TO_SPICLK(chip);
//uint8_t z = 0x00;
//ret = HAL_SPI_Transmit(chip->hspi,&z,3, 1000);
//SPI Reading Operation
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET);
ret = HAL_SPI_TransmitReceive(chip->hspi,data,rx,1, 1000);
HAL_SPI_change_clk_phase(chip, SPI_PHASE_1EDGE,SPI_POLARITY_HIGH);
ret = HAL_SPI_Receive(chip->hspi,rx+1,1, 1000);
ret = HAL_SPI_Receive(chip->hspi,rx+2,1, 1000);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_SET);
if(ret != HAL_OK){
return 1;
}
HAL_SPI_change_clk_phase(chip, SPI_PHASE_1EDGE, SPI_POLARITY_LOW);
HAL_SPICLK_TO_GPIO(chip);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_TO_SPICLK(chip);