Question
SPI max frequency test
Hey,
I would like to use an ADC LTC2315,
in maximum SPI interface (87.5Mhz Fclk).
Does anyone tried to work with the STM32H743 In SPI At this Frequency, or more?
From DS, in master mode Channel 1 can work in Max of 133MHz, hope it really does.
Moreover, can I work with 16 bit registers in SPI interface? I would like to run an algorithm on the Sampled data, hope I could work with 16 bit variable for better performance.