Skip to main content
SWenn.1
Senior III
March 13, 2022
Solved

SPI HAL receive command putting out 5 bytes worth of clock cycles ????

I have the following :

 HAL_SPI_Transmit(&hspi2, &txBuf[0], 1, 50);
 HAL_SPI_Receive(&hspi2, &rxBuf[0], 1, 50);

I have the following code .... STM32L476 is a spi 3 wire master. The Transmit appears (logic analyzer) to be working fine, however I am having much grief trying to read from the sensor (LSM6DSM33)....If I transmit two bytes with the second being a dummy byte of 0x00, the device responds with the appropriate response on the 3 wire connection. Unfortunately this method does not write anything into an rx buffer hence I THEN change to what you see above. The issue I am having is the above receive command puts 5 bytes worth of clocks out on the bus EVEN with a 1 as a parameter. If I put a 0 I get no clocks (as expected) and if I put a 2 I get (7 bytes worth of clocks). Can someone please explain what is going on????

This topic has been closed for replies.
TDK
TDKBest answer
March 13, 2022

RX only in bidirectional mode sends out clocks continuously. By the time the code catches up to realize a byte has already come in, a few more bytes have already been clocked.

Use four-wire mode if you can, or a lower clock speed.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
March 13, 2022

RX only in bidirectional mode sends out clocks continuously. By the time the code catches up to realize a byte has already come in, a few more bytes have already been clocked.

Use four-wire mode if you can, or a lower clock speed.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SWenn.1
SWenn.1Author
Senior III
March 13, 2022

Thank you

I have to use 3 wire as the end product is a sensorTile already wired up....Can you tell me is there ANY way to clock out 2 bytes with the TX command where the first is the register (with the Read bit set) and the second is a dummy to produce clocks with 0x00 from the STM. I seem to always see the sensor driving the MOSI line with the correct information when I do this BUT I just don't think there is a way to capture what it is sending in this mode???

TDK
March 13, 2022

With HAL and at very fast baud rates? Probably not. With your own code, or lower speeds, almost certainly.

If you can set the SPI to 16-bit mode then sending a word and immediately disabling RX mode will receive exactly one word.

The SPI RXONLY hardware implementation is awkward at best.

"If you feel a post has answered your question, please click ""Accept as Solution""."