Skip to main content
Associate III
November 21, 2024
Question

SPI DMA Transmission Starting from wrong address

Issue with SPI DMA Transmission Starting from Random Index Instead of Array Start (Circular Mode) (STM32L562VET6)

I am working with an STM32L562VET6 and have a 2D array DATA defined as follows:

 

uint8_t DATA[NOS][3] = {};

 

Here, NOS = 20000, and each row of this array contains a 24-bit integer value split into three bytes. For example:

 

DATA[3][0] = 0x00; 
DATA[3][1] = 0x00; 
DATA[3][2] = 0x03; 

 

 I’m transmitting this array using SPI with DMA in circular mode, like this:

 

HAL_SPI_Transmit_DMA(&hspi2, DATA, (uint16_t)(NOS * 3));

 

On the receiving side, I merge the three bytes back into a 24-bit integer. However, instead of the values starting from 0 (from DATA[0][0]), the transmission starts from some random index, goes up to 19999, and then wraps around to start again from 0 to the random starting index.

Why is the transmission not starting from DATA[0][0] in circular mode?
How can I ensure that the transmission always starts correctly from the beginning of the array?

Any insights or suggestions would be greatly appreciated! Thank you so much in advance!

This topic has been closed for replies.

1 reply

gbm
Super User
November 21, 2024

And what's the code for the receiving party? How do you ensure the the reception starts in sync with transmit?

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice