Skip to main content
Associate III
Jun 4, 2025 4:30 AM UTC
Solved

SPI communication using DMA on the STM32H743.

SPI communication using DMA on the STM32H743.

We have created a program for SPI communication using DMA, The first send/receive with HAL_SPI_TransmitReceive_DMA is successful.
However, when the exact same process is executed afterwards, all received values are 0.
The second send/receive with HAL_SPI_TransmitReceive_DMA is not successful.

Does anyone know why this is happening?

 

This topic has been closed for replies.
TDK
TDKBest answer
Jun 4, 2025 12:42 PM UTC

What are you talking to?

Can you verify on a logic analyzer that the data coming in is non-zero?

Are you managing cache appropriately or is it turned off?

What specifically makes you think all received values are zero?

How are you observing them?

Does HAL_SPI_TransmitReceive_DMA return HAL_OK and does the transfer complete callback get called?

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

Associate III
Jun 4, 2025 4:34 AM UTC

We are not sure if this is relevant, but I will post the SPI handle Structure values.

 

first dma_spi
hspi1	SPI_HandleTypeDef	{...}	
	Instance	SPI_TypeDef *	0x40013000	
		CR1	volatile uint32_t	0x1001	
		CR2	volatile uint32_t	0x0	
		CFG1	volatile uint32_t	0x70007	
		CFG2	volatile uint32_t	0x47400000	
		IER	volatile uint32_t	0x0	
		SR	volatile uint32_t	0x1002	
		IFCR	volatile uint32_t	0x0	
		RESERVED0	uint32_t	0x0	
		TXDR	volatile uint32_t	0x0	
		RESERVED1	uint32_t [3]	0x40013024	
			RESERVED1[0]	uint32_t	0x0	
			RESERVED1[1]	uint32_t	0x0	
			RESERVED1[2]	uint32_t	0x0	
		RXDR	volatile uint32_t	0x0	
		RESERVED2	uint32_t [3]	0x40013034	
			RESERVED2[0]	uint32_t	0x0	
			RESERVED2[1]	uint32_t	0x0	
			RESERVED2[2]	uint32_t	0x0	
		CRCPOLY	volatile uint32_t	0x107	
		TXCRC	volatile uint32_t	0x0	
		RXCRC	volatile uint32_t	0x0	
		UDRDR	volatile uint32_t	0x0	
		I2SCFGR	volatile uint32_t	0x0	
	Init	SPI_InitTypeDef	{...}	
		Mode	uint32_t	0x400000	
		Direction	uint32_t	0x0	
		DataSize	uint32_t	0x7	
		CLKPolarity	uint32_t	0x2000000	
		CLKPhase	uint32_t	0x1000000	
		NSS	uint32_t	0x4000000	
		BaudRatePrescaler	uint32_t	0x0	
		FirstBit	uint32_t	0x0	
		TIMode	uint32_t	0x0	
		CRCCalculation	uint32_t	0x0	
		CRCPolynomial	uint32_t	0x0	
		CRCLength	uint32_t	0x0	
		NSSPMode	uint32_t	0x40000000	
		NSSPolarity	uint32_t	0x0	
		FifoThreshold	uint32_t	0x0	
		TxCRCInitializationPattern	uint32_t	0x0	
		RxCRCInitializationPattern	uint32_t	0x0	
		MasterSSIdleness	uint32_t	0x0	
		MasterInterDataIdleness	uint32_t	0x0	
		MasterReceiverAutoSusp	uint32_t	0x0	
		MasterKeepIOState	uint32_t	0x0	
		IOSwap	uint32_t	0x0	
	pTxBuffPtr	const uint8_t *	0x0	
		*pTxBuffPtr	const uint8_t	0x40	
	TxXferSize	uint16_t	0x0	
	TxXferCount	volatile uint16_t	0x0	
	pRxBuffPtr	uint8_t *	0x0	
		*pRxBuffPtr	uint8_t	0x40	
	RxXferSize	uint16_t	0x0	
	RxXferCount	volatile uint16_t	0x0	
	CRCSize	uint32_t	0x0	
	RxISR	void (*)(struct __SPI_HandleTypeDef *)	0x0	
	TxISR	void (*)(struct __SPI_HandleTypeDef *)	0x0	
	hdmatx	DMA_HandleTypeDef *	0x240714a8	
		Instance	void *	0x40020058	
		Init	DMA_InitTypeDef	{...}	
			Request	uint32_t	0x26	
			Direction	uint32_t	0x40	
			PeriphInc	uint32_t	0x0	
			MemInc	uint32_t	0x400	
			PeriphDataAlignment	uint32_t	0x0	
			MemDataAlignment	uint32_t	0x0	
			Mode	uint32_t	0x0	
			Priority	uint32_t	0x10000	
			FIFOMode	uint32_t	0x0	
			FIFOThreshold	uint32_t	0x0	
			MemBurst	uint32_t	0x0	
			PeriphBurst	uint32_t	0x0	
		Lock	HAL_LockTypeDef	0x0	
		State	volatile HAL_DMA_StateTypeDef	0x1	
		Parent	void *	0x24071100	
		XferCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferHalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1CpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1HalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferErrorCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferAbortCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		ErrorCode	volatile uint32_t	0x0	
		StreamBaseAddress	uint32_t	0x40020000	
		StreamIndex	uint32_t	0x16	
		DMAmuxChannel	DMAMUX_Channel_TypeDef *	0x4002080c	
			CCR	volatile uint32_t	0x26	
		DMAmuxChannelStatus	DMAMUX_ChannelStatus_TypeDef *	0x40020880	
			CSR	volatile uint32_t	0x0	
			CFR	volatile uint32_t	0x0	
		DMAmuxChannelStatusMask	uint32_t	0x8	
		DMAmuxRequestGen	DMAMUX_RequestGen_TypeDef *	0x0	
			RGCR	volatile uint32_t	0x47868640	
		DMAmuxRequestGenStatus	DMAMUX_RequestGenStatus_TypeDef *	0x0	
			RGSR	volatile uint32_t	0x47868640	
			RGCFR	volatile uint32_t	0x25d3796f	
		DMAmuxRequestGenStatusMask	uint32_t	0x0	
	hdmarx	DMA_HandleTypeDef *	0x24071430	
		Instance	void *	0x40020040	
		Init	DMA_InitTypeDef	{...}	
			Request	uint32_t	0x25	
			Direction	uint32_t	0x0	
			PeriphInc	uint32_t	0x0	
			MemInc	uint32_t	0x400	
			PeriphDataAlignment	uint32_t	0x0	
			MemDataAlignment	uint32_t	0x0	
			Mode	uint32_t	0x0	
			Priority	uint32_t	0x10000	
			FIFOMode	uint32_t	0x0	
			FIFOThreshold	uint32_t	0x0	
			MemBurst	uint32_t	0x0	
			PeriphBurst	uint32_t	0x0	
		Lock	HAL_LockTypeDef	0x0	
		State	volatile HAL_DMA_StateTypeDef	0x1	
		Parent	void *	0x24071100	
		XferCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferHalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1CpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1HalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferErrorCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferAbortCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		ErrorCode	volatile uint32_t	0x0	
		StreamBaseAddress	uint32_t	0x40020000	
		StreamIndex	uint32_t	0x10	
		DMAmuxChannel	DMAMUX_Channel_TypeDef *	0x40020808	
			CCR	volatile uint32_t	0x25	
		DMAmuxChannelStatus	DMAMUX_ChannelStatus_TypeDef *	0x40020880	
			CSR	volatile uint32_t	0x0	
			CFR	volatile uint32_t	0x0	
		DMAmuxChannelStatusMask	uint32_t	0x4	
		DMAmuxRequestGen	DMAMUX_RequestGen_TypeDef *	0x0	
			RGCR	volatile uint32_t	0x47868640	
		DMAmuxRequestGenStatus	DMAMUX_RequestGenStatus_TypeDef *	0x0	
			RGSR	volatile uint32_t	0x47868640	
			RGCFR	volatile uint32_t	0x25d3796f	
		DMAmuxRequestGenStatusMask	uint32_t	0x0	
	Lock	HAL_LockTypeDef	0x0	
	State	volatile HAL_SPI_StateTypeDef	0x1	
	ErrorCode	volatile uint32_t	0x0	
txdata[0]	uint8_t	0x80	
txdata[1]	uint8_t	0x0	
txdata[2]	uint8_t	0x0	
txdata[3]	uint8_t	0x0	
txdata[4]	uint8_t	0x0	
txdata[5]	uint8_t	0x0	
second dma_spi
hspi1	SPI_HandleTypeDef	{...}	
	Instance	SPI_TypeDef *	0x40013000	
		CR1	volatile uint32_t	0x1000	
		CR2	volatile uint32_t	0x5	
		CFG1	volatile uint32_t	0x70007	
		CFG2	volatile uint32_t	0x47400000	
		IER	volatile uint32_t	0x0	
		SR	volatile uint32_t	0xe007	
		IFCR	volatile uint32_t	0x0	
		RESERVED0	uint32_t	0x0	
		TXDR	volatile uint32_t	0x0	
		RESERVED1	uint32_t [3]	0x40013024	
			RESERVED1[0]	uint32_t	0x0	
			RESERVED1[1]	uint32_t	0x0	
			RESERVED1[2]	uint32_t	0x0	
		RXDR	volatile uint32_t	0x0	
		RESERVED2	uint32_t [3]	0x40013034	
			RESERVED2[0]	uint32_t	0x0	
			RESERVED2[1]	uint32_t	0x0	
			RESERVED2[2]	uint32_t	0x0	
		CRCPOLY	volatile uint32_t	0x107	
		TXCRC	volatile uint32_t	0x0	
		RXCRC	volatile uint32_t	0x0	
		UDRDR	volatile uint32_t	0x0	
		I2SCFGR	volatile uint32_t	0x0	
	Init	SPI_InitTypeDef	{...}	
		Mode	uint32_t	0x400000	
		Direction	uint32_t	0x0	
		DataSize	uint32_t	0x7	
		CLKPolarity	uint32_t	0x2000000	
		CLKPhase	uint32_t	0x1000000	
		NSS	uint32_t	0x4000000	
		BaudRatePrescaler	uint32_t	0x0	
		FirstBit	uint32_t	0x0	
		TIMode	uint32_t	0x0	
		CRCCalculation	uint32_t	0x0	
		CRCPolynomial	uint32_t	0x0	
		CRCLength	uint32_t	0x0	
		NSSPMode	uint32_t	0x40000000	
		NSSPolarity	uint32_t	0x0	
		FifoThreshold	uint32_t	0x0	
		TxCRCInitializationPattern	uint32_t	0x0	
		RxCRCInitializationPattern	uint32_t	0x0	
		MasterSSIdleness	uint32_t	0x0	
		MasterInterDataIdleness	uint32_t	0x0	
		MasterReceiverAutoSusp	uint32_t	0x0	
		MasterKeepIOState	uint32_t	0x0	
		IOSwap	uint32_t	0x0	
	pTxBuffPtr	const uint8_t *	0x30000260	
		*pTxBuffPtr	const uint8_t	0x80	
	TxXferSize	uint16_t	0x5	
	TxXferCount	volatile uint16_t	0x0	
	pRxBuffPtr	uint8_t *	0x30000040	
		*pRxBuffPtr	uint8_t	0x0	
	RxXferSize	uint16_t	0x5	
	RxXferCount	volatile uint16_t	0x0	
	CRCSize	uint32_t	0x0	
	RxISR	void (*)(struct __SPI_HandleTypeDef *)	0x0	
	TxISR	void (*)(struct __SPI_HandleTypeDef *)	0x0	
	hdmatx	DMA_HandleTypeDef *	0x240714a8	
		Instance	void *	0x40020058	
		Init	DMA_InitTypeDef	{...}	
		Lock	HAL_LockTypeDef	0x0	
		State	volatile HAL_DMA_StateTypeDef	0x1	
		Parent	void *	0x24071100	
		XferCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferHalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1CpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1HalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferErrorCallback	void (*)(struct __DMA_HandleTypeDef *)	0x800fe6f	
		XferAbortCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		ErrorCode	volatile uint32_t	0x0	
		StreamBaseAddress	uint32_t	0x40020000	
		StreamIndex	uint32_t	0x16	
		DMAmuxChannel	DMAMUX_Channel_TypeDef *	0x4002080c	
		DMAmuxChannelStatus	DMAMUX_ChannelStatus_TypeDef *	0x40020880	
		DMAmuxChannelStatusMask	uint32_t	0x8	
		DMAmuxRequestGen	DMAMUX_RequestGen_TypeDef *	0x0	
		DMAmuxRequestGenStatus	DMAMUX_RequestGenStatus_TypeDef *	0x0	
		DMAmuxRequestGenStatusMask	uint32_t	0x0	
	hdmarx	DMA_HandleTypeDef *	0x24071430	
		Instance	void *	0x40020040	
		Init	DMA_InitTypeDef	{...}	
			Request	uint32_t	0x25	
			Direction	uint32_t	0x0	
			PeriphInc	uint32_t	0x0	
			MemInc	uint32_t	0x400	
			PeriphDataAlignment	uint32_t	0x0	
			MemDataAlignment	uint32_t	0x0	
			Mode	uint32_t	0x0	
			Priority	uint32_t	0x10000	
			FIFOMode	uint32_t	0x0	
			FIFOThreshold	uint32_t	0x0	
			MemBurst	uint32_t	0x0	
			PeriphBurst	uint32_t	0x0	
		Lock	HAL_LockTypeDef	0x0	
		State	volatile HAL_DMA_StateTypeDef	0x1	
		Parent	void *	0x24071100	
		XferCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x800fe0d	
		XferHalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x800fe53	
		XferM1CpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferM1HalfCpltCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		XferErrorCallback	void (*)(struct __DMA_HandleTypeDef *)	0x800fe6f	
		XferAbortCallback	void (*)(struct __DMA_HandleTypeDef *)	0x0	
		ErrorCode	volatile uint32_t	0x0	
		StreamBaseAddress	uint32_t	0x40020000	
		StreamIndex	uint32_t	0x10	
		DMAmuxChannel	DMAMUX_Channel_TypeDef *	0x40020808	
			CCR	volatile uint32_t	0x25	
		DMAmuxChannelStatus	DMAMUX_ChannelStatus_TypeDef *	0x40020880	
			CSR	volatile uint32_t	0x0	
			CFR	volatile uint32_t	0x0	
		DMAmuxChannelStatusMask	uint32_t	0x4	
		DMAmuxRequestGen	DMAMUX_RequestGen_TypeDef *	0x0	
			RGCR	volatile uint32_t	0x47868640	
		DMAmuxRequestGenStatus	DMAMUX_RequestGenStatus_TypeDef *	0x0	
			RGSR	volatile uint32_t	0x47868640	
			RGCFR	volatile uint32_t	0x25d3796f	
		DMAmuxRequestGenStatusMask	uint32_t	0x0	
	Lock	HAL_LockTypeDef	0x0	
	State	volatile HAL_SPI_StateTypeDef	0x1	
	ErrorCode	volatile uint32_t	0x0	
txdata[0]	uint8_t	0x80	
txdata[1]	uint8_t	0x0	
txdata[2]	uint8_t	0x0	
txdata[3]	uint8_t	0x0	
txdata[4]	uint8_t	0x0	
txdata[5]	uint8_t	0x0	
TDK
TDKBest answer
Jun 4, 2025 12:42 PM UTC

What are you talking to?

Can you verify on a logic analyzer that the data coming in is non-zero?

Are you managing cache appropriately or is it turned off?

What specifically makes you think all received values are zero?

How are you observing them?

Does HAL_SPI_TransmitReceive_DMA return HAL_OK and does the transfer complete callback get called?

"If you feel a post has answered your question, please click ""Accept as Solution""."
JBias
Associate III
Jun 5, 2025 11:46 PM UTC

I was seeing something similar on the STM32H7S3L8 except for me I was not getting the next callbacks unless I did a HAL_SPI_INIT as well as a HAL_DMA_INIT in between. Later I was able to reduce the time by optimizing out what was not needed. Of course, I would check the data stream coming in to verify that there is non-zero data as suggested by TDK

 

// HAL_SPI_Init(hspi);																//1. Verify SPI Initialization <-- works but too long
	SPI3->IER |= SPI_IER_RXPIE | SPI_IER_EOTIE; 									// Enable RX Packet Interrupt, End of Transfer Interrupt <--works instead of full HAL_SPI_Init(hspi)
// 	HAL_DMA_Init(&handle_HPDMA1_Channel15);										//2. Confirm DMA Configuration <-- works but too long
	if ((HPDMA1_Channel14->CFCR != 0 )|(handle_HPDMA1_Channel14.Lock != HAL_UNLOCKED)|(handle_HPDMA1_Channel14.State != HAL_DMA_STATE_READY)) {
		__HAL_DMA_DISABLE(&handle_HPDMA1_Channel14); 								//Disable DMA to allow register changes
		__HAL_DMA_RESET_HANDLE_STATE(&handle_HPDMA1_Channel14);						//Put into reset state to allow LOCK change todo needed ?
		__HAL_DMA_CLEAR_FLAG(&handle_HPDMA1_Channel14, (DMA_FLAG_TC | DMA_FLAG_HT | DMA_FLAG_DTE | DMA_FLAG_ULE | DMA_FLAG_USE | DMA_FLAG_SUSP |
									DMA_FLAG_TO));									//Clear all flags todo needed ?
		handle_HPDMA1_Channel14.Lock = HAL_UNLOCKED;								//Unlock
		handle_HPDMA1_Channel14.State = HAL_DMA_STATE_READY; 						//Ready State
		HPDMA1_Channel14->CCR |= DMA_CCR_EN; 										//Restart DMA
	}
	// Restart DMA for continuous reception
	volatile uint8_t *vBuffer = &gS2_RxData[0];										//8-bit buffer
	HAL_SPI_Receive_DMA(hspi, (uint8_t *)vBuffer, gS2_RxSize);						//DMA/SPI Start - Ready to receive