Skip to main content
Associate II
Apr 14, 2024 4:11 PM UTC
Question

SPI communication STM32H7B3I-DK

Hello everyone!

I am working on a project and using STM32H7B3I-DK board. I am facing issues with SPI communication. I am using simple code: 

while (1)

  {

    HAL_SPI_TransmitReceive(&hspi2, tx_data, rx_data, strlen(tx_data), HAL_MAX_DELAY); // Send AT command and receive response

    printf("Response: %s\r\n", rx_data); // Print received response

 

    HAL_Delay(1000); // Delay before sending the next command

  }

}

where after executing nothing is stored in rx_data. Do I need to modify clock configurations? 

Thanks in advance!

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
Apr 14, 2024 6:25 PM UTC

Hello,

You need to check if you're using the correct GPIOs and their configs that connect your MCU to the external device.

You need also to monitor your SPI lines with an oscilloscope or a logic analyzer. Are you seeing data coming back from the slave?

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.