Skip to main content
waclawek.jan
Super User
Feb 7, 2017 1:29 PM UTC
Solved

SPI BSY erratum listed under I2C in 'F76x/77x errata

Posted on February 07, 2017 at 14:29

In STM32F76xxx and STM32F77xxx silicon limitations DocID028806 Rev 4, 2.2.2  BSY bit may stay high at the end of a data transfer in slave mode which is entirely an SPI error, is listed under I2C peripheral limitations.

JW

    This topic has been closed for replies.
    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    Feb 7, 2017 3:16 PM UTC
    Posted on February 07, 2017 at 16:16

    Hi Jan,

    Thanks for keeping this error to our attention: I confirm that the limitation 'BSY bit may stay high at the end of a data transfer in slave mode' is misplaced and should belong to SPI limitations.

    This is noted and will be fixed in next errata version.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

    1 reply

    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    Feb 7, 2017 3:16 PM UTC
    Posted on February 07, 2017 at 16:16

    Hi Jan,

    Thanks for keeping this error to our attention: I confirm that the limitation 'BSY bit may stay high at the end of a data transfer in slave mode' is misplaced and should belong to SPI limitations.

    This is noted and will be fixed in next errata version.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.