Skip to main content
MagSense
Associate III
August 12, 2020
Question

SPI – bit shift issue in MISO line of STM32F303x (Slave) - with MOSI unaffected

Scenario –

Currently I am using STM32F303CBxx as my slave and an Infineon microcontroller as a master. The communication takes place via SPI with the clock frequency as high as 1.985 MHz (approx.). The master and slave are inside a closed metal compartment, where one of the control unit consumes higher amount of current, as high as 35 A.

Communication Protocol

The protocol for the communication is as follows.

0693W000003P8RHQA0.png 

Actual Communication and related issue

0693W000003P8RRQA0.png

From the above picture (measured data from picoscope), the decoded SPI message from the MISO line is as follows,

0x34 0x6F 0x00 0x12 0x38 0x77 0x1E 0x12

For CRC, I am using the XOR checksum (CRC8). When I check the above message for the validity (using a normal xor checksum calculator online), the xor byte becomes invalid (0x12)

Moreover, the expected message is as follows-> 0x34 0x6F 0x00 0x12 0x38 0x77 0x0F, with a CRC byte value of 0x09.

If I observe the 7th byte -> 0x1E -> 0001 1110, 1-bit shift happened towards the left, as the expected value was 0F -> 0000 1111. This bit shift happens at the 8th byte (CRC) as well.

12 (invalid CRC) -> 0001 0010 (measured) -> 0000 1001 (expected) -> 09 (valid CRC).

The bit-shifting issue happens only on the MISO line of the SPI, when the current consumption is on a higher range (more than 20 A, for example). The clock line does not get disturbed, as I always get valid messages on the MOSI. It should also be noted that the other functionalities of the slave (there are other measurements running in parallel) are unaffected.

This bit-shifting originates most of the time in the 7th or 8th byte of a packet, but rarely occurs in the 1st byte as well.

0693W000003P8WgQAK.png

For example, take a look into the above highlighted transaction.

The decoded MISO message is 0x60 0xAC 0x01 0xF0 0x01 0x96 0x04 0xAE. The complete packet is shifted to the left by exactly 1-bit. If I shift the message by 1-bit to the right, I receive the following message -> 0x30 0x56 0x00 0xF8 0x00 0xCB 0x02 0x57. This is a valid transaction and the message holds true.

What could be the source of such bit-shift error? Does this occur in the microcontroller itself?

Any recommendations regarding finding the source of such errors, are highly appreciated.

Please let me know if additional information is required.

Thank you.

This topic has been closed for replies.

38 replies

TDK
August 17, 2020

> But in theory, it is actually good to have a RC filter on communication lines like SPI, right?

I would not agree with this. Signaling doesn't need a filter unless you have a reason for it. With SPI, it can introduce clock skew. If your system has so much noise that a filter is necessary, perhaps differential signaling is required.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MagSense
MagSenseAuthor
Associate III
August 23, 2020

I agree with your answer. But the problem persists, even if I remove the filters (say from MISO/CLK lines). There were no difference in occurrences of errors.

TDK
August 23, 2020

So with the filter removed, you still have an SCK line that looks like a sine wave as in the original post?

"If you feel a post has answered your question, please click ""Accept as Solution""."