Skip to main content
Central SUPPORT
Senior
Sep 17, 2019 3:01 PM UTC
Solved

Source code included in STSW-STM32080 package for STM32 DfuSe utility

Product folder on st.com and databrief says "The STSW-STM32080 package contains all binaries and source code for DfuSe USB device firmware upgrade (DFU) software, including the demonstration, debugging GUIs, and protocol layers." Same is also mentioned in the readme.txt in the package.

I downloaded the package but could not find the sources in downloaded file. So, where are they?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This topic has been closed for replies.
Central SUPPORT
Central SUPPORTBest answer
Senior
Sep 26, 2019 2:51 PM UTC

Please note that for new STM32 products, it is recommended to use STM32CubeProgrammer.

2 replies

Central SUPPORT
Senior
Sep 17, 2019 3:02 PM UTC
  1. After download please launch DfuSe_Demo_V3.0.6_Setup.exe
  2. Once this installation has been done, all sources are available at this location (default setting): C:\Program Files (x86)\STMicroelectronics\Software\DfuSe v3.0.6\Sources

Central SUPPORT
Central SUPPORTAuthorBest answer
Senior
Sep 26, 2019 2:51 PM UTC

Please note that for new STM32 products, it is recommended to use STM32CubeProgrammer.