Skip to main content
Lagodolio
Associate III
Oct 23, 2018 10:19 AM UTC
Question

SOLVED - X Nucleo PLC01A1 : porting to F7

After writing some code for PLC01A1 and STM32 F446RE, I'm trying to port it on my F767ZI.

PLC Board uses SPI PA5, PA6 and PA7 for CLK, MISO and MOSI, and F4 & F7 have the same pinout.

In addition PLS01A1 uses F4's PB10,PB6 and PC7, but the same pins are named PE9,PD14 and PD15 on F7.

To sum:

F4 F7

B10 E9

B6 D14

C7 D15.

I changed x_nucleo_plc01a1.h given by STM so I have:

.....
 
#define X_NUCLEO_SPI_EXPBD_CLK_ENABLE() __SPI1_CLK_ENABLE()
#define X_NUCLEO_SPI_EXPBD_MISO_PIN GPIO_PIN_6
#define X_NUCLEO_SPI_EXPBD_MISO_PORT GPIOA
 
#define X_NUCLEO_SPI_EXPBD_MOSI_PIN GPIO_PIN_7
#define X_NUCLEO_SPI_EXPBD_MOSI_PORT GPIOA
 
#define X_NUCLEO_SPI_EXPBD_SCK_PIN GPIO_PIN_5
 
#define X_NUCLEO_SPI_EXPBD_SCK_PORT GPIOA
 
#define X_NUCLEO_TIM_PRESCALER 749
 
#define VNI8200XP_CS_CLK_ENABLE() __GPIOC_CLK_ENABLE();
#define VNI8200XP_CS_PIN GPIO_PIN_7
#define VNI8200XP_CS_PORT GPIOC
 
//NEW F7 Values
#define VNI8200XP_OUT_EN_CLK_ENABLE() __GPIOE_CLK_ENABLE();
#define VNI8200XP_OUT_EN_PIN GPIO_PIN_9
#define VNI8200XP_OUT_EN_PORT GPIOE
 
//OLD F4 Values
//#define VNI8200XP_OUT_EN_CLK_ENABLE() __GPIOB_CLK_ENABLE();
//#define VNI8200XP_OUT_EN_PIN GPIO_PIN_10
//#define VNI8200XP_OUT_EN_PORT GPIOB
 
 
//NEW F7 Values
#define CLT01_38S_CS_CLK_ENABLE() __GPIOD_CLK_ENABLE();
#define CLT01_38S_CS_PIN GPIO_PIN_14
#define CLT01_38S_CS_PORT GPIOD
 
//OLD F4 Values
//#define CLT01_38S_CS_CLK_ENABLE() __GPIOB_CLK_ENABLE();
//#define CLT01_38S_CS_PIN GPIO_PIN_6
//#define CLT01_38S_CS_PORT GPIOB
 
//NEW F7 Values
#define VNI8200XP_RESET_PORT GPIOD
#define VNI8200XP_RESET_PIN GPIO_PIN_15
 
#define VNI8200XP_ENABLE_PORT GPIOE
#define VNI8200XP_ENABLE_PIN GPIO_PIN_9
 
//OLD F4 Values
//#define VNI8200XP_RESET_PORT GPIOC
//#define VNI8200XP_RESET_PIN GPIO_PIN_7 
 
//#define VNI8200XP_ENABLE_PORT GPIOB
//#define VNI8200XP_ENABLE_PIN GPIO_PIN_10
 .....

The code (that is the same used for F4, with "f4xx*.h" headers substituted by "f7xx*.h") is correctly compiled but PLC doesn't work ...

GPIO B10,B6 &C7 seem used as generic GPIO, but PLC01A1 is declarated compatible with F1,F3 and F4 and F7 isn't named so: is it possible that xnucleo doesn't work on F7?

Thanks far all,

Mario

    This topic has been closed for replies.

    2 replies

    Lagodolio
    LagodolioAuthor
    Associate III
    Oct 23, 2018 2:11 PM UTC

    SOLVED!

    I didn't correct initial values...

    :o

    #define VNI8200XP_CS_CLK_ENABLE() __GPIOC_CLK_ENABLE();
    #define VNI8200XP_CS_PIN GPIO_PIN_7
    #define VNI8200XP_CS_PORT GPIOC

    Now I correct it with:

     //NEW F7 Values
    #define VNI8200XP_CS_CLK_ENABLE() __GPIOD_CLK_ENABLE();
    #define VNI8200XP_CS_PIN GPIO_PIN_15
    #define VNI8200XP_CS_PORT GPIOD
     
     //OLD F4 Values
    //#define VNI8200XP_CS_CLK_ENABLE() __GPIOC_CLK_ENABLE();
    //#define VNI8200XP_CS_PIN GPIO_PIN_7
    //#define VNI8200XP_CS_PORT GPIOC

    and works!!

    Visitor II
    Apr 28, 2024 8:26 PM UTC

    Hello,

    Recently I boy a X-Nucleo-PLC board and can't use the libraries from de examples. How and where can I start?