Skip to main content
Ciuffoly
Senior
December 3, 2019
Question

[SOLVED] -- very simple encoder ---

  • December 3, 2019
  • 0 replies
  • 446 views

Here my simple code to use the encoder on STM32F746.

I have used the PI2 and PI3 of the STM32F746G-DISCO for input and volume control on an external DAC.

Probably someone could reduce the lines of code and obtain the same result.

unsigned int Enc_dir; << output direction up/down to use in the main() or in
 handleTickEvent() in case of TouchGFX graphical interface
 environment.
unsigned int save_a = 0, save_b = 0; << global variables
 
 
void EXTI2_IRQHandler(void)
{
 uint8_t now_a;
 uint8_t now_b;
 
 
 HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_2);
 
 now_a = HAL_GPIO_ReadPin(GPIOI, GPIO_PIN_2);
 now_b = HAL_GPIO_ReadPin(GPIOI, GPIO_PIN_3);
 
 
 if (!save_a & !save_b)
 {
	if (now_a) 
	{
	 save_a = now_a;
	 Enc_dir = 2;
	}
	if (now_b) 
	{
	 save_b = now_b;
	 Enc_dir = 1;
	}
 }
 if (save_a & !save_b)
 {
	if (!now_a)
	{
	 save_a = now_a;
	 Enc_dir = 1;
	}
	if (now_b && now_a)
	{
	 save_b = now_b;
	 Enc_dir = 2;
	}
 }
 if (save_a & save_b)
 {
	if (!now_a)
	{
	 save_a = now_a;
	 Enc_dir = 2;
	}
	if (!now_b) 
	{
	 save_b = now_b;
	 Enc_dir = 1;
	}
 }
 if (!save_a & save_b)
 {
	if (now_a) 
 {
	 save_a = now_a;
	 Enc_dir = 1;
	}
	if (!now_b) 
 {
	 save_b = now_b;
	 Enc_dir = 2;
	}
 }
}
 
void BSP_Encoder_Init()
{
 GPIO_InitTypeDef gpio_init_structure;
 
 __HAL_RCC_GPIOI_CLK_ENABLE();
 
 gpio_init_structure.Pin = GPIO_PIN_2;
 gpio_init_structure.Mode = GPIO_MODE_IT_RISING_FALLING;
 gpio_init_structure.Pull = GPIO_PULLUP;
 
 HAL_GPIO_Init(GPIOI, &gpio_init_structure);
 
 HAL_NVIC_SetPriority(EXTI2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI2_IRQn);
 
 gpio_init_structure.Pin = GPIO_PIN_3;
 gpio_init_structure.Mode = GPIO_MODE_INPUT;
 gpio_init_structure.Pull = GPIO_PULLUP;
 
 HAL_GPIO_Init(GPIOI, &gpio_init_structure);
}

This topic has been closed for replies.